Hello NXP Community,
I’m working with the i.MX93 EVK and have connected a MIPI DSI-to-HDMI adapter board for video output. Upon booting from eMMC, I see four penguin icons in the upper left corner of the display, a Linux terminal icon on the top left, and a timer on the top right corner. However, neither my USB mouse nor keyboard is recognized:
- The mouse’s LED never lights up, indicating it’s not even getting power.
- There is no response from the keyboard, either.
I can still communicate with the board via a serial terminal (PuTTY), but I’d like to get a full graphical environment running with mouse and keyboard input. Has anyone encountered this behavior? Are there kernel configurations or device tree changes needed to enable USB peripherals on this EVK ? and if so what are these changes?
Any tips or insights would be greatly appreciated.
Thank you in advance!