i.MX93 EQoS RMII mode with internal 50MHz reference clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX93 EQoS RMII mode with internal 50MHz reference clock

跳至解决方案
803 次查看
jsopenrb
Contributor II

What is need to make EQoS work RMII mode with internal 50MHz reference clock?

Board init function in u-boot:

static int setup_eqos_rmii(void)
{
	struct blk_ctrl_wakeupmix_regs *bctrl =
		(struct blk_ctrl_wakeupmix_regs *)BLK_CTRL_WAKEUPMIX_BASE_ADDR;

	clrsetbits_le32(&bctrl->eqos_gpr,
			BCTRL_GPR_ENET_QOS_INTF_MODE_MASK,
			BCTRL_GPR_ENET_QOS_INTF_SEL_RMII | BCTRL_GPR_ENET_QOS_CLK_GEN_EN);

	return set_clk_eqos(ENET_50MHZ);
}

 

Relevant Linux dts parts, imx93-14x14-evk-tja1103.dts used as a basis for this config.

&eqos {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_eqos_rmii>;
        phy-mode = "rmii";
        phy-handle = <&eqosphy>;

        phy-reset-gpios = <&gpio4 17 GPIO_ACTIVE_LOW>;
        phy-reset-duration = <10>;

        assigned-clocks = <&clk IMX93_CLK_ENET_TIMER2>,
                        <&clk IMX93_CLK_ENET>;
        assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
                                <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>;
        assigned-clock-rates = <100000000>, <50000000>;

        clk_csr = <5>;
        status = "okay";

        mdio {
                compatible = "snps,dwmac-mdio";
                #address-cells = <1>;
                #size-cells = <0>;
                clock-frequency = <2500000>;
                eqosphy: ethernet-phy@0 {
                        reg = <0>;
                        compatible = "ethernet-phy-id0007.c0f0", "ethernet-phy-ieee802.3-c22";
                        smsc,disable-energy-detect;
                };
        };
};

...
&iomuxc { pinctrl_eqos_rmii: eqosrmiigrp { fsl,pins = < MX93_PAD_ENET1_TD2__CCM_ENET_QOS_CLOCK_GENERATE_REF_CLK 0x4000057e MX93_PAD_ENET1_MDC__ENET_QOS_MDC 0x57e MX93_PAD_ENET1_MDIO__ENET_QOS_MDIO 0x57e MX93_PAD_ENET1_RD0__ENET_QOS_RGMII_RD0 0x57e MX93_PAD_ENET1_RD1__ENET_QOS_RGMII_RD1 0x57e MX93_PAD_ENET1_RX_CTL__ENET_QOS_RGMII_RX_CTL 0x57e MX93_PAD_ENET1_TX_CTL__ENET_QOS_RGMII_TX_CTL 0x57e MX93_PAD_ENET1_TD1__ENET_QOS_RGMII_TD1 0x57e MX93_PAD_ENET1_TD0__ENET_QOS_RGMII_TD0 0x57e MX93_PAD_ENET2_TD2__GPIO4_IO17 0x31e >; }; ...

 

With the above configuration ethernet init fails with imx-dwmac 428a0000.ethernet: Failed to reset the dma

Any hints on what am I missing?

0 项奖励
回复
1 解答
782 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Please make these changes in your DTS.

assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
                         <&clk IMX93_CLK_SYS_PLL_PFD0_DIV2>;
assigned-clock-rates = <100000000>, <100000000>;

Patch your BSP with the patch below and the net: stmmac: dwmac-imx: use platform specific reset for imx93 SoCs:

diff --git a/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c b/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
index 2fb3fbbab7e5..7e001126243f 100644
--- a/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
+++ b/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
@@ -40,6 +40,8 @@
 #define MX93_GPR_ENET_QOS_INTF_SEL_RGMII (0x1 << 1)
 #define MX93_GPR_ENET_QOS_CLK_GEN_EN (0x1 << 0)
+#define MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL_MASK GENMASK(0, 0)
+#define MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL (0x1 << 0)
 struct imx_dwmac_ops {
 u32 addr_width;
 bool mac_rgmii_txclk_auto_adj;
@@ -54,7 +56,8 @@ struct imx_priv_data {
 struct regmap *intf_regmap;
 u32 intf_reg_off;
 bool rmii_refclk_ext;
-
+ struct regmap *enet_clk_sel_regmap;
+ u32 enet_clk_sel_off; const struct imx_dwmac_ops *ops;
 struct plat_stmmacenet_data *plat_dat;
 };
@@ -133,7 +136,27 @@ imx8dxl_set_intf_mode(struct plat_stmmacenet_data *plat_dat)
 static int imx93_set_intf_mode(struct plat_stmmacenet_data *plat_dat)
 {
 struct imx_priv_data *dwmac = plat_dat->bsp_priv;
- int val;
+ int val, err;
+
+ struct device_node *np = dwmac->dev->of_node;
+ if (plat_dat->interface == PHY_INTERFACE_MODE_RMII) {
+ dwmac->enet_clk_sel_regmap = syscon_regmap_lookup_by_phandle(np,
+ 
 "enet_clk_sel");
+ if (IS_ERR(dwmac->enet_clk_sel_regmap))
+ return PTR_ERR(dwmac->enet_clk_sel_regmap);
+
+ err = of_property_read_u32_index(np, "enet_clk_sel", 1,
+ &dwmac->enet_clk_sel_off);
+ if (err) {
+ dev_err(dwmac->dev,
+ "Can't get enet_clk_sel register offset
 (%d)\n",
+ err);
+ return err;
+ }
+ val = MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL;
+ regmap_update_bits(dwmac->enet_clk_sel_regmap, dwmac-
>enet_clk_sel_off,
+ MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL_MASK,
 val);
+ }
diff --git a/arch/arm64/boot/dts/freescale/imx93.dtsi b/arch/arm64/boot/dts/
freescale/imx93.dtsi
index 1f25503d421c..a4f8f841e2a7 100644
--- a/arch/arm64/boot/dts/freescale/imx93.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx93.dtsi
@@ -1079,6 +1079,8 @@
 <&clk
 IMX93_CLK_SYS_PLL_PFD0_DIV2>;
 assigned-clock-rates = <100000000>, <250000000>;
 intf_mode = <&wakeupmix_gpr 0x28>;
+ enet_clk_sel = <&wakeupmix_gpr 0x2C>;
+
 clk_csr = <0>;
 status = "disabled";
 };

Regards

在原帖中查看解决方案

0 项奖励
回复
3 回复数
656 次查看
jsopenrb
Contributor II

Small update. The DTS file must be modified like this to produce a 50MHz clock.

assigned-clock-rates = <100000000>, <50000000>;

 

0 项奖励
回复
783 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Please make these changes in your DTS.

assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>,
                         <&clk IMX93_CLK_SYS_PLL_PFD0_DIV2>;
assigned-clock-rates = <100000000>, <100000000>;

Patch your BSP with the patch below and the net: stmmac: dwmac-imx: use platform specific reset for imx93 SoCs:

diff --git a/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c b/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
index 2fb3fbbab7e5..7e001126243f 100644
--- a/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
+++ b/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.c
@@ -40,6 +40,8 @@
 #define MX93_GPR_ENET_QOS_INTF_SEL_RGMII (0x1 << 1)
 #define MX93_GPR_ENET_QOS_CLK_GEN_EN (0x1 << 0)
+#define MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL_MASK GENMASK(0, 0)
+#define MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL (0x1 << 0)
 struct imx_dwmac_ops {
 u32 addr_width;
 bool mac_rgmii_txclk_auto_adj;
@@ -54,7 +56,8 @@ struct imx_priv_data {
 struct regmap *intf_regmap;
 u32 intf_reg_off;
 bool rmii_refclk_ext;
-
+ struct regmap *enet_clk_sel_regmap;
+ u32 enet_clk_sel_off; const struct imx_dwmac_ops *ops;
 struct plat_stmmacenet_data *plat_dat;
 };
@@ -133,7 +136,27 @@ imx8dxl_set_intf_mode(struct plat_stmmacenet_data *plat_dat)
 static int imx93_set_intf_mode(struct plat_stmmacenet_data *plat_dat)
 {
 struct imx_priv_data *dwmac = plat_dat->bsp_priv;
- int val;
+ int val, err;
+
+ struct device_node *np = dwmac->dev->of_node;
+ if (plat_dat->interface == PHY_INTERFACE_MODE_RMII) {
+ dwmac->enet_clk_sel_regmap = syscon_regmap_lookup_by_phandle(np,
+ 
 "enet_clk_sel");
+ if (IS_ERR(dwmac->enet_clk_sel_regmap))
+ return PTR_ERR(dwmac->enet_clk_sel_regmap);
+
+ err = of_property_read_u32_index(np, "enet_clk_sel", 1,
+ &dwmac->enet_clk_sel_off);
+ if (err) {
+ dev_err(dwmac->dev,
+ "Can't get enet_clk_sel register offset
 (%d)\n",
+ err);
+ return err;
+ }
+ val = MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL;
+ regmap_update_bits(dwmac->enet_clk_sel_regmap, dwmac-
>enet_clk_sel_off,
+ MX93_ENET_CLK_ENET_QOS_TX_CLK_SEL_MASK,
 val);
+ }
diff --git a/arch/arm64/boot/dts/freescale/imx93.dtsi b/arch/arm64/boot/dts/
freescale/imx93.dtsi
index 1f25503d421c..a4f8f841e2a7 100644
--- a/arch/arm64/boot/dts/freescale/imx93.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx93.dtsi
@@ -1079,6 +1079,8 @@
 <&clk
 IMX93_CLK_SYS_PLL_PFD0_DIV2>;
 assigned-clock-rates = <100000000>, <250000000>;
 intf_mode = <&wakeupmix_gpr 0x28>;
+ enet_clk_sel = <&wakeupmix_gpr 0x2C>;
+
 clk_csr = <0>;
 status = "disabled";
 };

Regards

0 项奖励
回复
420 次查看
fuyutang
Contributor I

we also have the similar problem,no 50MHz clock output from CPU MAC,if somewhere wrong ? thanks20241101-174056.jpg20241101-174106.jpg

0 项奖励
回复