i.MX8mplus imx-image-full qt6 demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8mplus imx-image-full qt6 demo

1,089 次查看
coilnpark
Contributor IV

Dear all,

 

I got i.MX8mplus kit and I tried to run qt6 demo.

Even I excuted demo application, it didn't work.

Anyboy can help me?

0 项奖励
3 回复数

1,062 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

QT6 is on 5.15.5 kernel, Honister Yocto, Qt 6 is built into the Linux image in the Yocto Project environment with the command bitbake imx-image-full. For more details on Qt enablement, check out
the README in the meta-imx repo and the i.MX Yocto Project User's Guide.

Regards

0 项奖励

1,041 次查看
coilnpark
Contributor IV

Even I tested it as  L5.15.52-2.1.0, it didn't work.

0 项奖励

1,053 次查看
coilnpark
Contributor IV

Hi~

I installed L5.15.32_2.0.0

0 项奖励