i.MX8m-mini DRAM Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8m-mini DRAM Controller

ソリューションへジャンプ
1,852件の閲覧回数
JamesShih
Contributor III

Hi,

I followed the linux ref manual 2.5.4 and able to control the bus frequency, but it seems like not control the DRAM controller directly, correct?

If yes, what if I would like to control the DRAM Controller directly? Or I can do both at the same time?

Thanks.

James Shih

ラベル(1)
0 件の賞賛
返信
1 解決策
1,818件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @JamesShih

NXP vendor tree is using a private busfreq [1] driver to do ddr and bus fabric scalling rather than using upstream ddrc & interconnect
driver which is still immature. And actually there's no i.MX driver users of ICC in current vendor kernel. So removing them in order to avoid confusing to customers

B.R

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,819件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @JamesShih

NXP vendor tree is using a private busfreq [1] driver to do ddr and bus fabric scalling rather than using upstream ddrc & interconnect
driver which is still immature. And actually there's no i.MX driver users of ICC in current vendor kernel. So removing them in order to avoid confusing to customers

B.R

0 件の賞賛
返信
1,807件の閲覧回数
JamesShih
Contributor III
Thanks, it's clear for me now.
0 件の賞賛
返信
1,847件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @JamesShih 

What do you mean control the DRAM Controller directly? please explain more details

B.R

0 件の賞賛
返信
1,834件の閲覧回数
JamesShih
Contributor III
Hi Pengyong,

Sorry for the incomplete information, the DRAM Controller I mean is the DDR Controller.

Right now in my environment, I'm able to use "busfreq" to set DDR and NOC to the lower frequency and for sure able to see the power consumption going down.

Beside, there is another one called "devfreq", I tried to enable it in my environment, but unfortunately it didn't work and even not able to see the node.

To clarify my question, I just want to confirm if in the same clock (lower frequency) condition by either busfreq or devfreq, from the power consumption point of view it shouldn't be any different, correct?

Hopefully it's clear for you to understand my question, thanks.
0 件の賞賛
返信