i.MX8dxl eqos ethernet fixed-link: Failed to reset the dma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8dxl eqos ethernet fixed-link: Failed to reset the dma

Jump to solution
6,223 Views
catwich
Contributor I

\o/

We are trying to enable the second network port (ENET1) on a custom i.MX8dxl board, with lf-5.15.5-1.0.0.
However we encounter somewhat obscure error messages on the console when trying to bring up a link:

 

root@2a473698774a:~# ip link set dev eth0 up
[  166.341902] imx-dwmac 5b050000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[  167.355265] imx-dwmac 5b050000.ethernet: Failed to reset the dma
[  167.361354] imx-dwmac 5b050000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[  167.370371] imx-dwmac 5b050000.ethernet eth0: stmmac_open: Hw setup failed
RTNETLINK answers: Connection timed out

 

 
I noticed many questions about similar errors on the i.MX8M Plus - but they are (probably) not applicable in our case because we want to connect directly to an SJA1110a switch using rgmii without a dedicated phy in between.

Our board shares a lot with the EVK, e.g. we can boot the imx8dxl-evk.dtb and try enabling the eqos interface (after replacing the phy with fixed-link in dts) - and still trigger the same error.
So for reference below are the relevant parts of our device-tree, which includes imx8dxl.dtsi at its base:

 

&iomuxc {
        pinctrl_eqos: eqosgrp {
            fsl,pins = <
                /* MDIO to Switch */
                IMX8DXL_ENET0_MDC_CONN_EQOS_MDC             0x06000020
                IMX8DXL_ENET0_MDIO_CONN_EQOS_MDIO           0x06000020
                /* RGMII to Switch */
                IMX8DXL_ENET1_RGMII_TX_CTL_CONN_EQOS_RGMII_TX_CTL   0x06000020
                IMX8DXL_ENET1_RGMII_TXC_CONN_EQOS_RGMII_TXC     0x06000020
                IMX8DXL_ENET1_RGMII_TXD0_CONN_EQOS_RGMII_TXD0       0x06000020
                IMX8DXL_ENET1_RGMII_TXD1_CONN_EQOS_RGMII_TXD1       0x06000020
                IMX8DXL_ENET1_RGMII_TXD2_CONN_EQOS_RGMII_TXD2       0x06000020
                IMX8DXL_ENET1_RGMII_TXD3_CONN_EQOS_RGMII_TXD3       0x06000020
                IMX8DXL_ENET1_RGMII_RXC_CONN_EQOS_RGMII_RXC     0x06000020
                IMX8DXL_ENET1_RGMII_RX_CTL_CONN_EQOS_RGMII_RX_CTL   0x06000020
                IMX8DXL_ENET1_RGMII_RXD0_CONN_EQOS_RGMII_RXD0       0x06000020
                IMX8DXL_ENET1_RGMII_RXD1_CONN_EQOS_RGMII_RXD1       0x06000020
                IMX8DXL_ENET1_RGMII_RXD2_CONN_EQOS_RGMII_RXD2       0x06000020
                IMX8DXL_ENET1_RGMII_RXD3_CONN_EQOS_RGMII_RXD3       0x06000020
            >;
        };
};

&eqos {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_eqos>;
    phy-mode = "rgmii-id";
    status = "okay";

    fixed-link {
        speed = <1000>;
        full-duplex;
    };
};

 


Also please find the full boot log attached ...

0 Kudos
Reply
1 Solution
6,146 Views
catwich
Contributor I

With assistance from NXP we were able to work out the issues from my post above - and do now have rx&tx operating properly between the switch and the SoC eqos.

Essentially the eqos controller requires the rx clock to operate dma.
If anyone else faces this issue - verify that the connected phy or switch provides a clock to the SoC ENET1_RGMII_RXC input.

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
6,147 Views
catwich
Contributor I

With assistance from NXP we were able to work out the issues from my post above - and do now have rx&tx operating properly between the switch and the SoC eqos.

Essentially the eqos controller requires the rx clock to operate dma.
If anyone else faces this issue - verify that the connected phy or switch provides a clock to the SoC ENET1_RGMII_RXC input.

Tags (1)
0 Kudos
Reply