I am looking for a spot on the iMX8X OTP (or other on-chip non-volatile storage) to store roughly 64 8bit device identifier values.
After reviewing the Fusemap table (Table 7-1) in the IMX8X reference manual I am only seeing two words available for "Customer" use, along with a few bits here and there (Customer_OTP_word0 and Customer_OTP_word1, plus Customer_OTP_bit[7:0]).
After reading the section "7.2 Fusemap", I noticed that it mentions "The indexes from 272 to 543 are not being used", my question is if those indexes are not used should they be considered "reserved" or should I consider them as free to be used for my own purposes?
Solved! Go to Solution.
Hello,
Please consider them as reserved do not use them.
Best regards,
Aldo.
Hello,
Please consider them as reserved do not use them.
Best regards,
Aldo.