i.MX8X LPDDR4 ZQ_RESISTOR_SHARED question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8X LPDDR4 ZQ_RESISTOR_SHARED question

Jump to solution
1,155 Views
m_c
Senior Contributor I

How to set ZQ_RESISTOR_SHARED in the Register Script Aids for below LPDDR4 connection?

 

 

ZQ_RESISTOR_SHARED

-

0

00000000

Description: Shared ZQ resistor between ranks.
■ 1 - Denotes that ZQ resistor is shared between ranks. Means ZQinit/ZQCL/ZQCS commands are sent to one rank at a time with tZQinit/tZQCL/tZQCS timing met between commands so that commands to different ranks do not overlap.
■ 0 - ZQ resistor is not shared.
Value After Reset: 0x0

 

 
 
0 Kudos
1 Solution
1,144 Views
igorpadykov
NXP Employee
NXP Employee

Hi m_c

 

one can refer  to below answer:

https://community.nxp.com/t5/i-MX-Processors/Shared-ZQ-resistor/m-p/953291

If you use two-rank LPDDR4 and have two ZQ resistors, you set it to DISABLED.

 

Best regards
igor

View solution in original post

0 Kudos
1 Reply
1,145 Views
igorpadykov
NXP Employee
NXP Employee

Hi m_c

 

one can refer  to below answer:

https://community.nxp.com/t5/i-MX-Processors/Shared-ZQ-resistor/m-p/953291

If you use two-rank LPDDR4 and have two ZQ resistors, you set it to DISABLED.

 

Best regards
igor

0 Kudos