i.MX8QuadMax TRM and cfg file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QuadMax TRM and cfg file

933件の閲覧回数
ranjith_tc
Contributor I

I have recently bought.i.MX8QuadMax MEK CPU board. Is it possible to get the OPenOCD cfg file for this board?

Or is it possible to get the TRM of i.MX8QMAX processor, so that i could fing the debug and cti base addresses and DAP ID? Unable to find the TRM from the NXP website is annoying.

ラベル(1)
0 件の賞賛
返信
1 返信

880件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

for debug one can follow AN12631

Normal and Secure Debug for i.MX8/8X Family of Applications Processors

(unfortunately I am not aware of OPenOCD cfg files). TRM of i.MX8QMAX processor

can be obtained in local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信