i.MX8QXP memtester failed to run problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP memtester failed to run problem

Jump to solution
2,863 Views
zhengguang_yang
Contributor II
Hi 
We are using imx8qxp, Yocto3.0.
Kernel Version:5.4.70
We found that on the imx8qxp yocto 3.0 system, if the parameters behind the memtester are greater than 50% of the DDR free space, the system will kill the memtester because of insufficient memory.
1.png
As shown in the figure above, the available space is 1.2G. Execute the command memtester 700M, the system will report the following error, and then kill memtester.
2.png
We found that Yocto 3.0 system on i.MX8MM platform does not have this problem, and Yocto 2.5 system on i.MX8QXP platform does not have this problem.
Only Yocto 3.0 system on i.MX8QXP platform has this problem.
0 Kudos
Reply
1 Solution
2,832 Views
josephzhou1
Contributor V

hi , all

1

i.MX8QXP EVK? i tok it is i.MX8QXP MEK???

2

 

i saw his board is i.MX8X RTX 2.1

josephzhou1_0-1641952199275.png

is not supported . then you must port in your board.

 

3

We found that Yocto 3.0 system on i.MX8MM platform does not have this problem, so imx8MQ also ok  but i saw " memtester not tainted" , try Bitbake by yours self? 

4

as mentioned , we suggest that you use Yocto BSP 3.1 which is a Long Term Support version itself

thank you , Solved.

Dunfell3.1April 20203.1.13 (Dec. 2021)Long Term Support (until Apr. 2024)

 

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore

View solution in original post

5 Replies
2,785 Views
charleshuang
Senior Contributor II

Hi @Rita_Wang and NXP teams,

We found that the Imx8mq evk board also has the problem on the 5.4.70 Yocto 3.0 demo image.

The 4.14.98 Yocto 2.5 and 5.10.9 Yocto 3.2 demo images on the Imx8mq evk board does not have this problem.

Could you please help to verify the 5.4.70 Yocto 3.0 BSP? Thanks.

charleshuang_0-1641948652280.png

 

0 Kudos
Reply
2,775 Views
josephzhou1
Contributor V

as mentioned , we suggest that you use Yocto BSP 3.1 which is a Long Term Support version itself

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply
2,814 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can see the Yocto release version align with the code https://wiki.yoctoproject.org/wiki/Releases.

How about the 3.1version using?

0 Kudos
Reply
2,835 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP i.MX8QXP EVK board?

0 Kudos
Reply
2,833 Views
josephzhou1
Contributor V

hi , all

1

i.MX8QXP EVK? i tok it is i.MX8QXP MEK???

2

 

i saw his board is i.MX8X RTX 2.1

josephzhou1_0-1641952199275.png

is not supported . then you must port in your board.

 

3

We found that Yocto 3.0 system on i.MX8MM platform does not have this problem, so imx8MQ also ok  but i saw " memtester not tainted" , try Bitbake by yours self? 

4

as mentioned , we suggest that you use Yocto BSP 3.1 which is a Long Term Support version itself

thank you , Solved.

Dunfell3.1April 20203.1.13 (Dec. 2021)Long Term Support (until Apr. 2024)

 

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore