i.MX8QXP clock gating method

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX8QXP clock gating method

304 Views
Contributor IV

Hi, community.

We have a question about how to clock gating to reduce power consumption.

We use i.MX8QXP w/ L4.14.98_2.0.0.

We are trying clock gating to further reduce the power consumption of MX8QXP. It was confirmed that the power consumption was slightly reduced by turning off the following resource subdomain.
If you don't use these resources, I think it's okay to leave it off, is that OK?

- Display Controller (we don't use DC)

 SC_R_DC_0,

    SC_R_DC_0_PLL_0,

    SC_R_DC_0_PLL_1

- CM4  (we don't use CM4)

   SC_R_M4_0_INTMUX

   SC_R_M4_0_MU_1A

- VPU ( we don't use MJPEG encoder.)

   SC_R_MJPEG_ENC_S0

 

Reference source:

* SCFW Porting Kit Documents

(sc_fw_api_qx_bo.pdf)

* System Controller Firmware

i.MX 8 System Controller Unit and System Controller Firmware Overview 

System Controller Firmware 101 

* System Controller Firmware command line interface

scfw_cli - System Controller Firmware command line interface 

Best Regards,

kanou

0 Kudos
2 Replies

32 Views
Contributor IV

Hi Diego,

I was able to turn off each resource using the device tree instead of scfw_cli.

I decided that the risk was high by using scfw_cli, so I decided to turn off these resources in the device tree.
Thanks, anyway.

32 Views
NXP Employee
NXP Employee

Hello,

I am working on your problem. However, due to the difficulty of the problem, this may take some time.

Best regards,

Diego.

0 Kudos