i.MX8QXP capture raw(bayer) data and debayer doc question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP capture raw(bayer) data and debayer doc question

614 Views
xu_ji1
Contributor V

Hello,

About this doc in community

i.MX8QXP capture raw(bayer) data and debayer

I use the patch that raw capture test and #include "g2d.h"

but when I build the program,it happened build error can not get g2d.h

what is the correct path?

0 Kudos
4 Replies

530 Views
xu_ji1
Contributor V

Hello,

How to fix the patch build error?

0 Kudos

530 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

one can look at Software ISP Application Note 

https://www.nxp.com/docs/en/application-note/AN12060.pdf 

gtec-demo-framework/DemoApps/OpenCL/SoftISP at master · NXPmicro/gtec-demo-framework · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

530 Views
xu_ji1
Contributor V

I want to use the test application get Raw image,but now the code build error

0 Kudos

530 Views
xu_ji1
Contributor V

Hi,

I said this imx8_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff patch build error not softISP,

please help the build error

0 Kudos