i.MX8QXP: Howto load and start SPL image via uuu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QXP: Howto load and start SPL image via uuu

1,390件の閲覧回数
Niebel-TQ
Contributor IV

We try to bringup uuu for our own boards. Current Version of uuu is able to download an start SCU firmware and SPL. Loading the second AP Container (ATF + U-Boot.img) works afterwards using

uuu sdpv: write -f u-boot-atf-container.img

But starting the container using

uuu sdpv: jump

fails. The same image (flash.bin) can be flashed on board and boots to U-Boot prompt.
U-Boot version: based on u-boot-imx branch lf-5.4.y_v2019.04

ラベル(1)
0 件の賞賛
返信
1 返信

1,373件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, Mueller,

uuu does not support only writing spl to the onboard flash.

B.R,

Weidong

0 件の賞賛
返信