i.MX8QXP: Howto load and start SPL image via uuu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP: Howto load and start SPL image via uuu

1,394 Views
Niebel-TQ
Contributor IV

We try to bringup uuu for our own boards. Current Version of uuu is able to download an start SCU firmware and SPL. Loading the second AP Container (ATF + U-Boot.img) works afterwards using

uuu sdpv: write -f u-boot-atf-container.img

But starting the container using

uuu sdpv: jump

fails. The same image (flash.bin) can be flashed on board and boots to U-Boot prompt.
U-Boot version: based on u-boot-imx branch lf-5.4.y_v2019.04

0 Kudos
Reply
1 Reply

1,377 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, Mueller,

uuu does not support only writing spl to the onboard flash.

B.R,

Weidong

0 Kudos
Reply