i.MX8QM looking for Coresight base addresses (debug, CTI, ETM, ...) for processor probe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM looking for Coresight base addresses (debug, CTI, ETM, ...) for processor probe

Jump to solution
2,283 Views
ToarteFretter
Senior Contributor I

Hi,

To be able to manually setup a processor probe for debugging on the i.MX8QM, we need several parameters for the many cores inside (A72, A53, M4), parameters like: APB index, Memmap type, Debug base address, CTI base address, ETM base address, ... .

Where can we find this information, or is there somebody that can provide us with this information for the many CPU cores inside?

Thanks!

Kind regards, ToarteFretter.

0 Kudos
Reply
1 Solution
2,252 Views
ToarteFretter
Senior Contributor I

Hi Igor,

The links are not really providing the base addresses that I need, but the ZIP-file that you provided me via email does!

Many thanks.

Regards,

ToarteFretter.

View solution in original post

0 Kudos
Reply
4 Replies
2,253 Views
ToarteFretter
Senior Contributor I

Hi Igor,

The links are not really providing the base addresses that I need, but the ZIP-file that you provided me via email does!

Many thanks.

Regards,

ToarteFretter.

0 Kudos
Reply
2,266 Views
igorpadykov
NXP Employee
NXP Employee

Hi ToarteFretter

 

one can look at AN12631  Normal and Secure Debug for i.MX8/8X Family of Applications Processors

and lauterbach debug scripts on

https://www.lauterbach.com/frames.html?scripts.html?Terms=IMX8QUADMAX

 

Best regards
igor

0 Kudos
Reply
2,230 Views
sinanakman
Senior Contributor III

Igor, can you please send that zip file to me as well.

Thanks

Sinan Akman

0 Kudos
Reply
2,205 Views
sinanakman
Senior Contributor III

@igorpadykov, can you please send that zip file for scripts or would you like me to open a support ticket for this.

Please let me know

Regards

Sinan Akman

An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----