i.MX8QM display problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM display problem

2,155 Views
cptb
Contributor I

I encountered the problem of screen probability performance lighting, hope someone can help solve, using i.MX8QM development board and RM67191 screen. When I burned the Android tablet image, the screen was normal and could be lit up 100%. When I burned the car image, the screen was lit up with probability and the display image was rotated 90 degrees. The car image should have used two switching boards, lvds-to-hdmi and mipi-to-hdmi. I removed the adapter board driver and device tree directly using the mipi screen display. Attempts to modify the screen parameters and modify the rotation parameter of drm_plane did not solve the problem.

[    8.453102][  T236] random: init: uninitialized urandom read (40 bytes read)
[    8.483181][  T236] random: init: uninitialized urandom read (40 bytes read)
[    8.490710][  T236] random: init: uninitialized urandom read (4 bytes read)
[    8.598901][  T237] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.
v33: No such file or directory
[    8.610362][  T237] linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.
v33: No such file or directory
[    8.625025][  T237] linkerconfig (237) used greatest stack depth: 11112 bytes left
[    8.668069][  T238] ueventd: ueventd started!
[    8.675794][  T238] selinux: SELinux: Loaded file_contexts
[    8.681342][  T238] selinux: 
[    8.685456][  T238] ueventd: Parsing file /system/etc/ueventd.rc...
[    8.691919][  T238] ueventd: Added '/vendor/etc/ueventd.rc' to import list
[    8.698849][  T238] ueventd: Added '/odm/etc/ueventd.rc' to import list
[    8.705987][  T238] ueventd: Parsing file /vendor/etc/ueventd.rc...
[    8.711027][  T239] apexd: Bootstrap subcommand detected
[    8.713159][  T238] ueventd: /vendor/etc/ueventd.rc: 42: /sys/ lines must have 5 or 6 entries
[    8.717683][  T239] apexd: ActivateFlattenedApex
[    8.726366][  T238] ueventd: Parsing file /odm/etc/ueventd.rc...
[    8.730900][  T239] apexd: Scanning /system/apex
[    8.736861][  T238] ueventd: Unable to read config file '/odm/etc/ueventd.rc': open() failed:
 No such file or directory
[    8.741956][  T239] apexd: Bind mounting /system/apex/com.android.adbd onto /apex/com.android
.adbd
[    8.762248][  T239] apexd: Bind mounting /system/apex/com.android.adservices onto /apex/com.a
ndroid.adservices
[    8.773021][  T239] apexd: Bind mounting /system/apex/com.android.appsearch onto /apex/com.an
droid.appsearch
[    8.783619][  T239] apexd: Bind mounting /system/apex/com.android.art onto /apex/com.android.
art
[    8.793930][  T239] apexd: Bind mounting /system/apex/com.android.btservices onto /apex/com.a
ndroid.btservices
[    8.804962][  T239] apexd: Bind mounting /system/apex/com.android.car.framework onto /apex/co
m.android.car.framework
[    8.816344][  T239] apexd: Bind mounting /system/apex/com.android.cellbroadcast onto /apex/co
m.android.cellbroadcast
[    8.854382][  T239] printk: apexd: 26 output lines suppressed due to ratelimiting
[    9.097141][  T241] <unknown>: getrandom indicates that the entropy pool has not been initial
ized. Rather than continue with poor entropy, this process will block until entropy is available
.
[    9.658561][    C1] random: crng init done
[    9.662687][    C1] random: 38 urandom warning(s) missed due to ratelimiting
[    9.720426][  T241] boringssl_self_ (241) used greatest stack depth: 10992 bytes left
[    9.821188][  T249] boringssl_self_ (249) used greatest stack depth: 10968 bytes left
[    9.871181][   T58] audit: type=1400 audit(1689388936.796:4): avc:  denied  { sys_admin } for
  pid=250 comm="init.insmod.sh" capability=21  scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-
insmod-sh:s0 tclass=capability permissive=0
[    9.917814][  T253] setprop (253) used greatest stack depth: 10816 bytes left
[   10.085073][  T256] module built by bfz at 2023年 07月 17日 星期一 10:09:47 CST
[   10.087489][  T256] Galcore version 6.4.3.p4.398061
[   10.121825][  T256] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu1_ss on min
or 0
[   10.122752][    T1] Registered swp emulation handler
[   10.166813][  T251] binder: 251:251 transaction failed 29189/-22, size 0-0 line 2920
[   10.199529][  T260] Hot alarm is canceled. GPU3D clock will return to 64/64
[   10.213003][  T261] logd.auditd: start
[   10.217328][  T261] logd.klogd: 10118762375
[   10.228145][  T271] watchdogd: watchdogd started (interval 10, margin 20)!
mek_8q:/ $ [   10.253153][  T261] logd: Loaded bug_map file: /vendor/etc/selinux/selinux_denial_
metadata
[   10.262805][  T261] logd: Loaded bug_map file: /system/etc/selinux/bug_map
[   10.620001][  T298] send message failed!
[   10.624301][  T298] send message failed!
[   10.628526][  T298] send message failed!
[   10.632730][  T298] send message failed!
[   10.636873][  T298] send message failed!
[   10.641059][  T298] send message failed!
[   10.645209][  T298] send message failed!
[   10.649352][  T298] send message failed!
[   10.653455][  T298] send message failed!
[   10.657554][  T298] send message failed!
[   10.661698][  T298] send message failed!
[   10.665948][  T298] send message failed!
[   10.670116][  T298] send message failed!
[   10.674285][  T298] send message failed!
[   10.678423][  T298] send message failed!
[   10.682627][  T298] send message failed!
[   10.686805][  T298] send message failed!
[   10.691204][  T298] send message failed!
[   10.695497][  T298] send message failed!
[   10.699650][  T298] send message failed!
[   10.703796][  T298] send message failed!
[   10.707926][  T298] send message failed!
[   10.712172][  T298] send message failed!
[   10.716422][  T298] send message failed!
[   10.720547][  T298] send message failed!
[   10.724729][  T298] send message failed!
[   10.729025][  T298] send message failed!
[   10.733075][  T298] send message failed!
[   10.737118][  T298] send message failed!
[   10.741202][  T298] send message failed!
[   10.745246][  T298] send message failed!
[   10.749290][  T298] send message failed!
[   10.753313][  T298] send message failed!
[   10.757366][  T298] send message failed!
[   10.761423][  T298] send message failed!
[   10.765455][  T298] send message failed!
[   10.769026][  T277] fsck.f2fs: Info: Fix the reported corruption.
[   10.769482][  T298] send message failed!
[   10.775597][  T277] fsck.f2fs: Info: not exist /proc/version!
[   10.779560][  T298] send message failed!
[   10.785289][  T277] fsck.f2fs: Info: Segments per section = 1
[   10.789339][  T298] send message failed!
[   10.795049][  T277] fsck.f2fs: Info: Sections per zone = 1
[   10.799060][  T298] send message failed!
[   10.804833][  T277] fsck.f2fs: Info: sector size = 4096
[   10.808571][  T298] send message failed!
[   10.813817][  T277] fsck.f2fs: Info: total sectors = 2257408 (8818 MB)
[   10.817838][  T298] send message failed!
[   10.824357][  T277] fsck.f2fs: Info: MKFS version
[   10.828377][  T298] send message failed!
[   10.833074][  T277] fsck.f2fs:   "5.15.71-g279b46e22312-dirty"
[   10.837093][  T298] send message failed!
[   10.842972][  T277] fsck.f2fs: Info: FSCK version
[   10.846909][  T298] send message failed!
[   10.851598][  T277] fsck.f2fs:   from "5.15.71-g279b46e22312-dirty"
[   10.855531][  T298] send message failed!
[   10.865951][  T298] send message failed!
[   10.870004][  T298] send message failed!
[   10.874091][  T298] send message failed!
[   10.878158][  T298] send message failed!
[   10.882234][  T298] send message failed!
[   10.886324][  T298] send message failed!
[   10.890354][  T298] send message failed!
[   10.894422][  T298] send message failed!
[   10.899099][  T298] send message failed!
[   10.903295][  T298] send message failed!
[   10.907334][  T298] send message failed!
[   10.911392][  T298] send message failed!
[   10.915373][  T298] send message failed!
[   10.919392][  T298] send message failed!
[   10.923473][  T298] send message failed!
[   10.927534][  T298] send message failed!
[   10.931573][  T298] send message failed!
[   10.935603][  T298] send message failed!
[   10.939667][  T298] send message failed!
[   10.943742][  T298] send message failed!
[   10.947821][  T298] send message failed!
[   10.951911][  T298] send message failed!
[   10.955995][  T298] send message failed!
[   10.960080][  T298] send message failed!
[   10.964222][  T298] send message failed!
[   10.968294][  T298] send message failed!
[   10.972387][  T298] send message failed!
[   10.976434][  T298] send message failed!
[   10.980526][  T298] send message failed!
[   10.984586][  T298] send message failed!
[   10.988709][  T298] send message failed!
[   10.992825][  T298] send message failed!
[   10.996952][  T298] send message failed!
[   11.001023][  T298] send message failed!
[   11.005102][  T298] send message failed!
[   11.009189][  T298] send message failed!
[   11.013275][  T298] send message failed!
[   11.017370][  T298] send message failed!
[   11.021590][  T298] send message failed!
[   11.025621][  T298] send message failed!
[   11.029664][  T298] send message failed!
[   11.033646][  T298] send message failed!
[   11.037632][  T298] send message failed!
[   11.041604][  T298] send message failed!
[   11.045589][  T298] send message failed!
[   11.049570][  T298] send message failed!
[   11.053569][  T298] send message failed!
[   11.057647][  T298] send message failed!
[   11.061737][  T298] send message failed!
[   11.065844][  T298] send message failed!
[   11.070288][  T298] send message failed!
[   11.074500][  T298] send message failed!
[   11.078607][  T298] send message failed!
[   11.083135][  T298] send message failed!
[   11.087286][  T298] send message failed!
[   11.091463][  T298] receive power state report with value 0
[   11.097631][  T298] send message failed!
[   11.101855][  T298] send message failed!
[   11.105864][  T298] send message failed!
[   11.109870][  T298] send message failed!
[   11.114268][  T298] send message failed!
[   11.118319][  T298] send message failed!
[   11.122381][  T298] send message failed!
[   11.126528][  T298] send message failed!
[   11.130601][  T298] send message failed!
[   11.134777][  T298] send message failed!
[   11.139090][  T298] send message failed!
[   11.143115][  T298] send message failed!
[   11.147194][  T298] send message failed!
[   11.151277][  T298] send message failed!
[   11.155363][  T298] send message failed!
[   11.159416][  T298] send message failed!
[   11.163466][  T298] send message failed!
[   11.167508][  T298] send message failed!
[   11.171556][  T298] send message failed!
[   11.175542][  T298] send message failed!
[   11.179542][  T298] send message failed!
[   11.183534][  T298] send message failed!
[   11.187527][  T298] send message failed!
[   11.191527][  T298] send message failed!
[   11.195530][  T298] send message failed!
[   11.199561][  T298] send message failed!
[   11.203594][  T298] send message failed!
[   11.207603][  T298] send message failed!
[   11.211625][  T298] send message failed!
[   11.521304][   T10] imx6q-pcie 5f000000.pcie: No cache used with register defaults set!
[   11.566654][   T10] imx6q-pcie 5f000000.pcie: PCIe PLL is locked.
[   11.573002][   T10] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[   11.579313][   T10] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[   11.587612][   T10] imx6q-pcie 5f000000.pcie: host bridge /bus@5f000000/pcie@0x5f000000 range
s:
[   11.596392][   T10] imx6q-pcie 5f000000.pcie:       IO 0x006ff80000..0x006ff8ffff -> 0x000000
0000
[   11.605299][   T10] imx6q-pcie 5f000000.pcie:      MEM 0x0060000000..0x006fefffff -> 0x006000
0000
[   11.614271][   T10] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[   11.620598][   T10] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[   12.626596][   T10] imx6q-pcie 5f000000.pcie: Phy link never came up
[   12.634177][   T10] imx6q-pcie: probe of 5f000000.pcie failed with error -110
[   12.688251][  T277] F2FS-fs (dm-10): Using encoding defined by superblock: utf8-12.1.0 with f
lags 0x0
[   12.718300][  T277] F2FS-fs (dm-10): Mounted with checkpoint version = 7a83d964
[   12.863726][  T281] type=1400 audit(1689388939.788:5): avc: denied { sys_admin } for comm="an
droid.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0
 tclass=capability permissive=0
[   12.883902][  T281] type=1400 audit(1689388939.788:6): avc: denied { sys_admin } for comm="an
droid.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0
 tclass=capability permissive=0
[   12.934845][    T1] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
[   13.087351][  T277] vold: keystore2 Keystore earlyBootEnded returned service specific error: 
-68
[   13.183246][  T274] logd: logd reinit
[   13.190651][  T274] logd: FrameworkListener: read() failed (Connection reset by peer)
[   13.191432][  T388] apexd: This device does not support updatable APEX. Exiting
[   13.205991][  T388] apexd: Marking APEXd as activated
[   13.236631][  T201] debugfs: File 'Playback' in directory 'dapm' already present!
[   13.244211][  T201] debugfs: File 'Capture' in directory 'dapm' already present!
[   13.263000][    T1] init: Not setting encryption policy on: /data/system_ce
[   13.270408][    T1] init: Not setting encryption policy on: /data/misc_de
[   13.277587][    T1] init: Not setting encryption policy on: /data/misc_ce
[   13.284789][    T1] init: Not setting encryption policy on: /data/user
[   13.291799][    T1] init: Not setting encryption policy on: /data/user_de
[   13.299593][    T1] init: Command 'rm /data/user/0' action=post-fs-data (/system/etc/init/hw/
init.rc:915) took 0ms and failed: unlink() failed: Is a directory
[   13.333149][    T1] init: Verified that /data/cache has the encryption policy bb09fc91faf1e41
246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.347340][    T1] init: Verified that /data/rollback has the encryption policy bb09fc91faf1
e41246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.360443][    T1] init: Verified that /data/rollback-observer has the encryption policy bb0
9fc91faf1e41246d6bf58c43996d1 v2 modes 1/4 flags 0xa
[   13.373669][    T1] init: Inferred action different from explicit one, expected 2 but got 3
[   13.434891][  T394] cs42xx8 1-0048: failed to get device ID, ret = -1
[   13.442164][  T394] cs42xx8: probe of 1-0048 failed with error -1
[   13.568915][  T399] fec 5b040000.ethernet: Adding to iommu group 2
[   13.578147][  T399] pps pps0: new PPS source ptp0
[   13.595367][  T399] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing.
[   13.607256][  T399] fec 5b040000.ethernet eth0: registered PHC device 0
[   13.718197][  T403] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   13.727146][  T403] cfg80211: Problem loading in-kernel X.509 certificate (-13)
[   13.727598][  T281] type=1400 audit(1689388940.652:7): avc: denied { write } for comm="insmod
" scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-insmod-sh:s0 tclass=key permissive=0
[   13.753221][  T155] cfg80211: loaded regulatory.db is malformed or signature is missing/inval
id
[   13.753586][  T281] type=1400 audit(1689388940.676:8): avc: denied { search } for comm="kwork
er/1:10" scontext=u:r:kernel:s0 tcontext=u:r:init-insmod-sh:s0 tclass=key permissive=0
[   13.879670][  T409] apexd: This device does not support updatable APEX. Exiting
[   13.887053][  T409] apexd: Marking APEXd as ready
[   13.916838][  T410] mlan: loading out-of-tree module taints kernel.
[   13.999929][    T1] WARNING: Unprivileged eBPF is enabled, data leaks possible via Spectre v2
 BHB attacks!
[   14.036780][  T412] wlan: Loading MWLAN driver
[   14.042104][  T412] wlan: Register to Bus Driver...
[   14.049974][  T412] wlan: Register to Bus Driver Done
[   14.055122][  T412] wlan: Driver loaded successfully
[   14.062952][  T415] LibBpfLoader: Section bpfloader_min_ver value is 2 [0x2]
[   14.070304][  T415] LibBpfLoader: Section bpfloader_max_ver value is 65536 [0x10000]
[   14.078338][  T415] LibBpfLoader: Section size_of_bpf_map_def value is 116 [0x74]
[   14.085972][  T415] LibBpfLoader: Section size_of_bpf_prog_def value is 92 [0x5c]
[   14.093550][  T415] LibBpfLoader: BpfLoader version 0x00013 processing ELF object /apex/com.a
ndroid.tethering/etc/bpf/offload.o with ver [0x00002,0x10000)
[   14.134527][  T417] remoteproc remoteproc1: imx-dsp-rproc is available
[   15.944403][  T415] printk: bpfloader: 1679 output lines suppressed due to ratelimiting
[   15.993543][  T429] update_verifier: Started with arg 1: nonencrypted
[   16.003542][  T429] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[   16.010727][  T429] update_verifier: Leaving update_verifier.
[   16.100693][  T236] Mass Storage Function, version: 2009/09/11
[   16.106618][  T236] LUN: removable file: (no medium)
[   16.116711][  T236] using random self ethernet address
[   16.121969][  T236] using random host ethernet address
[   16.128026][  T236] file system registered
[   16.383345][  T454] healthd: No battery devices found
[   16.411578][  T454] healthd: battery none chg=u
[   16.541126][  T281] type=1400 audit(1689388943.464:9): avc: denied { read } for comm="android
.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontrol
_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   16.602873][  T281] type=1400 audit(1689388943.528:10): avc: denied { integrity } for comm="i
nit" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown 
permissive=0
[   16.621508][  T281] type=1400 audit(1689388943.528:11): avc: denied { integrity } for comm="i
nit" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown 
permissive=0
[   16.847979][  T497] amphion-vpu-core 2d090000.vpu-core: encoder firmware version : 1.3.3
[   16.884900][  T497] amphion-vpu-core 2d080000.vpu-core: decoder firmware version : 1.8.6
[   17.473082][  T570] read descriptors
[   17.476768][  T570] read strings
[   18.342478][  T172] android_work: sent uevent USB_STATE=CONNECTED
[   18.351560][  T172] android_work: sent uevent USB_STATE=CONFIGURED
[   18.411905][  T272] logd: logdr: UID=1036 GID=1007 PID=566 b tail=0 logMask=bf pid=0 start=16
89388918381464000ns deadline=0ns
[   20.824179][  T281] type=1400 audit(1689388947.748:12): avc: denied { read } for comm="main" 
name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=318 scontext=u:r:zygote:s0 tcontext=u:o
bject_r:vendor_default_prop:s0 tclass=file permissive=0
[   21.575624][  T281] type=1400 audit(1689388948.500:13): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   24.598150][    T1] init: service 'idmap2d' requested start, but it is already running (flags
: 4)
[   24.607211][    T1] init: Control message: Processed ctl.start for 'idmap2d' from pid: 619 (s
ystem_server)
[   24.794386][  T454] healthd: battery none chg=u
[   25.224294][    T1] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/system/et
c/init/hw/init.rc:1193)
[   25.235860][    T1] init: starting service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)'
...
[   25.251181][    T1] init: SVC_EXEC service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)'
 pid 710 (uid 0 gid 0+0 context default) started; waiting...
[   25.650192][    T1] init: Service 'exec 19 (/system/bin/extra_free_kbytes.sh 24300)' (pid 710
) exited with status 0 waiting took 0.402000 seconds
[   25.663523][    T1] init: Sending signal 9 to service 'exec 19 (/system/bin/extra_free_kbytes
.sh 24300)' (pid 710) process group...
[   25.675956][    T1] libprocessgroup: Successfully killed process cgroup uid 0 pid 710 in 0ms
[   26.166030][  T691] read descriptors
[   26.169768][  T691] read strings
[   26.173248][  T691] read descriptors
[   26.176922][  T691] read strings
[   26.567414][  T431] Qualcomm Atheros AR8031/AR8033 5b040000.ethernet-1:00: attached PHY drive
r (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
[   26.584608][  T281] type=1400 audit(1689388953.508:14): avc: denied { read } for comm="main" 
name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=318 scontext=u:r:zygote:s0 tcontext=u:o
bject_r:vendor_default_prop:s0 tclass=file permissive=0
[   26.610659][  T281] type=1400 audit(1689388953.532:15): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   28.459475][  T281] type=1400 audit(1689388955.384:16): avc: granted { read } for comm="rksta
ck.process" name="psched" dev="proc" ino=4026531994 scontext=u:r:network_stack:s0 tcontext=u:obj
ect_r:proc_net:s0 tclass=file
[   28.482878][  T281] type=1400 audit(1689388955.404:17): avc: granted { read open } for comm="
rkstack.process" path="/proc/878/net/psched" dev="proc" ino=4026531994 scontext=u:r:network_stac
k:s0 tcontext=u:object_r:proc_net:s0 tclass=file
[   28.506009][  T281] type=1400 audit(1689388955.404:18): avc: granted { getattr } for comm="rk
stack.process" path="/proc/878/net/psched" dev="proc" ino=4026531994 scontext=u:r:network_stack:
s0 tcontext=u:object_r:proc_net:s0 tclass=file
[   28.592879][  T313] send message failed!
[   28.647104][  T313] send message failed!
[   28.660177][  T313] send message failed!
[   28.666762][  T313] receive power state report with value 0
[   28.672776][  T313] send message failed!
[   29.109733][    T1] init: processing action (boot.car_service_created=1) from (/system/etc/in
it/com.android.car.procfsinspector.rc:7)
[   29.124773][    T1] init: starting service 'com.android.car.procfsinspector'...
[   29.178070][  T313] send message failed!
[   31.686098][  T281] type=1400 audit(1689388958.608:19): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   32.012042][    T1] init: processing action (sys.boot_completed=1) from (/system/etc/init/hw/
init.rc:1184)
[   32.023583][    T1] init: starting service 'exec 21 (/bin/rm -rf /data/per_boot)'...
[   32.038386][    T1] init: SVC_EXEC service 'exec 21 (/bin/rm -rf /data/per_boot)' pid 1541 (u
id 1000 gid 1000+0 context default) started; waiting...
[   32.073214][    T1] init: Service 'exec 21 (/bin/rm -rf /data/per_boot)' (pid 1541) exited wi
th status 0 waiting took 0.036000 seconds
[   32.086741][    T1] init: Sending signal 9 to service 'exec 21 (/bin/rm -rf /data/per_boot)' 
(pid 1541) process group...
[   32.098826][    T1] libprocessgroup: Successfully killed process cgroup uid 1000 pid 1541 in 
0ms
[   32.115874][    T1] init: Encryption policy of /data/per_boot set to 96a81c4fc373aab9cf654b0d
1b75c442 v2 modes 1/4 flags 0xa
[   32.130190][    T1] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/
init.nxp.rc:199)
[   32.182408][    T1] init: processing action (sys.boot_completed=1) from (/vendor/etc/init/hw/
init.nxp.imx8qm.rc:48)
[   32.219000][    T1] init: processing action (sys.boot_completed=1 && vendor.all.car=true) fro
m (/vendor/etc/init/hw/init.nxp.imx8qm.rc:86)
[   32.249040][  T236] vehicle_rpmsg virtio0.rpmsg-vehicle-channel.-1.1: new channel: 0x401 -> 0
x1!
[   32.264864][  T172] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[   32.277474][  T172] debugfs: Directory 'img-pdma1' with parent 'pm_genpd' already present!
[   32.288410][  T172] debugfs: Directory 'img-pdma2' with parent 'pm_genpd' already present!
[   32.299195][  T172] debugfs: Directory 'img-pdma3' with parent 'pm_genpd' already present!
[   32.308639][  T172] debugfs: Directory 'img-pdma4' with parent 'pm_genpd' already present!
[   32.324046][  T172] debugfs: Directory 'img-pdma5' with parent 'pm_genpd' already present!
[   32.332710][  T172] debugfs: Directory 'img-pdma6' with parent 'pm_genpd' already present!
[   32.342487][  T172] debugfs: Directory 'img-pdma7' with parent 'pm_genpd' already present!
[   32.409980][  T172] imx-lpi2c 57247000.i2c: use pio mode
[   32.416717][  T172] i2c 5-004c: Fixing up cyclic dependency with bus@57240000:ldb@572410e0
[   33.434963][  T172] it6263 5-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[   33.443357][  T172] i2c i2c-5: LPI2C adapter registered
[   33.631745][  T172] platform 57180000.dpu: Fixing up cyclic dependency with 57228000.dsi_host
[   33.646186][  T172] dpu-core 57180000.dpu: driver probed
[   33.648094][  T176] ***************************bfz panel probe in****************************
****
[   33.663385][  T176] panel-raydium-rm67191 57228000.dsi_host.0: nonexclusive access to GPIO fo
r reset
[   33.672966][  T176] panel-raydium-rm67191 57228000.dsi_host.0: supply v3p3 not found, using d
ummy regulator
[   33.683382][  T176] panel-raydium-rm67191 57228000.dsi_host.0: supply v1p8 not found, using d
ummy regulator
[   33.694077][  T176] nwl-dsi 57228000.dsi_host: [drm:nwl_dsi_host_attach [nwl_dsi]] lanes=4, f
ormat=0x0 flags=0x215
[   33.704847][  T176] ******************bfz panel probe out*******************
[   33.720512][  T172] imx-lpi2c 58226000.i2c: use pio mode
[   33.722774][  T176] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_o
ps)
[   33.732080][  T172] i2c i2c-6: LPI2C adapter registered
[   33.759307][  T176] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_o
ps)
[   33.763631][  T172] imx-lpi2c 58246000.i2c: use pio mode
[   33.778712][  T172] i2c i2c-7: LPI2C adapter registered
[   33.785635][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[   33.787776][  T172] mxc-md bus@58000000:camera: deferring cap_device registration
[   33.800816][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[   33.806048][  T172] isi-capture 58100000.isi:cap_device: deferring 58100000.isi:cap_device de
vice registration
[   33.815564][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[   33.822275][  T172] isi-m2m 58100000.isi:m2m_device: deferring 58100000.isi:m2m_device device
 registration
[   33.839672][  T172] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[   33.847599][  T176] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[   33.849134][  T172] isi-capture 58110000.isi:cap_device: deferring 58110000.isi:cap_device de
vice registration
[   33.866133][  T176] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component
_ops [nwl_dsi])
[   33.877255][  T172] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[   33.878484][  T176] imx-drm display-subsystem: bound bus@56240000:ldb@562410e0 (ops imx8qm_ld
b_ops [imx8qm_ldb])
[   33.910021][  T172] isi-capture 58120000.isi:cap_device: deferring 58120000.isi:cap_device de
vice registration
[   33.920573][  T176] imx-drm display-subsystem: bound 57228000.dsi_host (ops nwl_dsi_component
_ops [nwl_dsi])
[   33.931166][  T172] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[   33.938971][  T176] imx-drm display-subsystem: bound bus@57240000:ldb@572410e0 (ops imx8qm_ld
b_ops [imx8qm_ldb])
[   33.947884][  T172] isi-capture 58130000.isi:cap_device: deferring 58130000.isi:cap_device de
vice registration
[   33.960103][  T176] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[   33.964036][  T172] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[   33.977996][  T182] vref_1v8: disabling
[   33.982066][  T182] SD3_SPWR: disabling
[   33.983082][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   33.987150][  T172] isi-capture 58140000.isi:cap_device: deferring 58140000.isi:cap_device de
vice registration
[   33.999702][  T176] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[   34.004170][  T172] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[   34.021500][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   34.021852][  T172] isi-capture 58150000.isi:cap_device: deferring 58150000.isi:cap_device de
vice registration
[   34.029823][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   34.039017][  T172] mxc-isi 58150000.isi: mxc_isi.5 registered successfully
[   34.046786][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   34.055112][  T172] isi-capture 58160000.isi:cap_device: deferring 58160000.isi:cap_device de
vice registration
[   34.061178][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video6
[   34.070442][  T172] mxc-isi 58160000.isi: mxc_isi.6 registered successfully
[   34.077559][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   34.086727][  T172] isi-capture 58170000.isi:cap_device: deferring 58170000.isi:cap_device de
vice registration
[   34.102526][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   34.103175][  T172] mxc-isi 58170000.isi: mxc_isi.7 registered successfully
[   34.110598][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   34.124447][  T172] platform 58227000.csi: Fixing up cyclic dependency with 6-006a
[   34.127573][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   34.139316][  T496] audit: audit_lost=1 audit_rate_limit=5 audit_backlog_limit=64
[   34.139461][  T281] type=1400 audit(1689388961.064:20): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.141010][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video6
[   34.141640][  T176] mx8-img-md: Registered mxc_isi.4.capture as /dev/video7
[   34.142079][  T176] mx8-img-md: Registered mxc_isi.5.capture as /dev/video8
[   34.142468][  T176] mx8-img-md: Registered mxc_isi.6.capture as /dev/video9
[   34.142705][  T176] mxc-md bus@58000000:camera: deferring cap_device registration
[   34.146950][  T496] audit: rate limit exceeded
[   34.154797][  T172] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[   34.169902][  T176] max9286_mipi 6-006a: max9286_read_reg:read reg error: reg=1e
[   34.171461][  T281] type=1400 audit(1689388961.064:21): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173321][  T281] type=1400 audit(1689388961.064:22): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173466][  T281] type=1400 audit(1689388961.064:23): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173564][  T281] type=1400 audit(1689388961.064:24): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173660][  T281] type=1400 audit(1689388961.064:25): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173755][  T281] type=1400 audit(1689388961.064:26): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173866][  T281] type=1400 audit(1689388961.064:27): avc: denied { search } for comm="HwBi
nder:453_2" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tcontex
t=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.173962][  T281] type=1400 audit(1689388961.064:28): avc: denied { search } for comm="HWC-
Poll-Thread" name="data" dev="dm-10" ino=98 scontext=u:r:hal_graphics_composer_default:s0 tconte
xt=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   34.180179][  T172] platform 58247000.csi: Fixing up cyclic dependency with 7-006a
[   34.184169][  T176] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[   34.271942][  T172] mxc-mipi-csi2 58247000.csi: lanes: 4, name: mxc-mipi-csi2.1
[   34.361424][  T176] max9286_mipi 7-006a: max9286_read_reg:read reg error: reg=1e
[   34.392585][  T172] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video3 (81,3
)
[   34.406777][  T176] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[   34.417690][  T172] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video4 (81,4
)
[   34.423138][  T176] mx8-img-md: Registered mxc_isi.0.capture as /dev/video5
[   34.469391][  T176] mx8-img-md: Registered mxc_isi.1.capture as /dev/video6
[   34.477536][  T176] mx8-img-md: Registered mxc_isi.2.capture as /dev/video7
[   34.516172][  T176] mx8-img-md: Registered mxc_isi.3.capture as /dev/video8
[   34.524003][  T176] mx8-img-md: Registered mxc_isi.4.capture as /dev/video9
[   34.531574][  T176] mx8-img-md: Registered mxc_isi.5.capture as /dev/video10
[   34.563754][  T176] mx8-img-md: Registered mxc_isi.6.capture as /dev/video11
[   34.571512][  T176] mx8-img-md: Registered mxc_isi.7.capture as /dev/video12
[   34.580859][  T176] unregister ISI channel: mxc_isi.0
[   34.586795][  T176] unregister ISI channel: mxc_isi.1
[   34.592453][  T176] unregister ISI channel: mxc_isi.2
[   34.598333][  T176] unregister ISI channel: mxc_isi.3
[   34.604250][  T176] unregister ISI channel: mxc_isi.4
[   34.614715][  T176] unregister ISI channel: mxc_isi.5
[   34.621148][  T176] unregister ISI channel: mxc_isi.6
[   34.627237][  T176] unregister ISI channel: mxc_isi.7
[   34.947670][  T496] ***************************bfz panel init in*****************************
***
[   34.996076][ T1730] ci_hdrc ci_hdrc.0: EHCI Host Controller
[   35.001736][ T1730] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[   35.022647][ T1730] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[   35.026609][  T496] ***************************bfz panel init out****************************
****
[   35.029089][ T1730] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice=
 5.15
[   35.046751][ T1730] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   35.055284][ T1730] usb usb1: Product: EHCI Host Controller
[   35.060927][ T1730] usb usb1: Manufacturer: Linux 5.15.71-g279b46e22312-dirty ehci_hcd
[   35.068879][ T1730] usb usb1: SerialNumber: ci_hdrc.0
[   35.074644][ T1730] hub 1-0:1.0: USB hub found
[   35.079185][ T1730] hub 1-0:1.0: 1 port detected
[   35.100542][ T1730] insmod (1730) used greatest stack depth: 9600 bytes left
[   35.607695][  T496] ***************************bfz panel init in*****************************
***
[   35.686601][  T496] ***************************bfz panel init out****************************
****
[   36.756565][  T281] type=1400 audit(1689388963.680:61): avc: denied { read } for comm="androi
d.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=98 scontext=u:r:hal_audiocontro
l_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   38.547308][  T644] binder_alloc: 2009: binder_alloc_buf, no vma
[   38.555262][  T644] binder: 619:644 transaction failed 29189/-3, size 3564-8 line 3101
[   40.961761][    T1] init: Sending signal 9 to service 'idmap2d' (pid 533) process group...
[   40.981303][    T1] libprocessgroup: Successfully killed process cgroup uid 1000 pid 533 in 1
1ms
[   40.994891][    T1] init: Control message: Processed ctl.stop for 'idmap2d' from pid: 619 (sy
stem_server)
[   41.004826][  T643] binder_alloc: 2394: binder_alloc_buf, no vma
[   41.005509][    T1] init: Service 'idmap2d' (pid 533) received signal 9
[   41.011670][  T643] binder: 619:643 transaction failed 29189/-3, size 88-0 line 3101
[   45.862907][  T619] binder_alloc: 3159: binder_alloc_buf, no vma
[   45.879346][  T619] binder: 619:619 transaction failed 29189/-3, size 136-0 line 3101
[   56.382579][    C2] Unable to handle kernel paging request at virtual address dead00000000012
a
[   56.382643][   T20] Kernel panic - not syncing: CFI failure (target: rad_panel_probe.9c599efe
498b8cff52ce0fab43b5b106.cfi_jt+0x0/0x4)
[   56.391242][    C2] Mem abort info:
[   56.403250][   T20] SMP: stopping secondary CPUs
[   56.411363][    C2]   ESR = 0x96000044
[   56.415115][    C2]   EC = 0x25: DABT (current EL), IL = 32 bits
[   56.421127][    C2]   SET = 0, FnV = 0
[   56.424879][    C2]   EA = 0, S1PTW = 0
[   56.428720][    C2]   FSC = 0x04: level 0 translation fault
[   56.434297][    C2] Data abort info:
[   56.437876][    C2]   ISV = 0, ISS = 0x00000044
[   56.442411][    C2]   CM = 0, WnR = 1
[   56.446077][    C2] [dead00000000012a] address between user and kernel address ranges
[   56.453916][    C2] Internal error: Oops: 96000044 [#1] PREEMPT SMP
[   56.460199][    C2] Modules linked in: ci_hdrc_imx(E) usbmisc_imx(E) ci_hdrc(E) ulpi(E) snd_s
of_imx8(E) imx_common(E) snd_sof_xtensa_dsp(E) snd_sof_of(E) snd_sof(E) imx_dsp_rproc(E) moal(OE
) mlan(OE) mac80211(E) cfg80211(E) fec(E) at803x(E) snd_soc_cs42xx8_i2c(E) snd_soc_cs42xx8(E) sn
d_soc_fsl_esai(E) snd_soc_bt_sco(E) spi_slave_system_control(E) spi_slave_time(E) spi_imx(E) spi
_fsl_lpspi(E) spi_bitbang(E) spidev(E) pci_imx6(E) phy_fsl_imx8_pcie(E) snd_soc_fsl_sai(E) imx_p
cm_dma(E) snd_soc_fsl_asoc_card(E) snd_soc_imx_audmux(E) snd_soc_simple_card(E) snd_soc_simple_c
ard_utils(E) snd_soc_wm8960(E) mx3fb(E) fb_fence(E) mxc_edid(E) cfbimgblt(E) cfbcopyarea(E) cfbf
illrect(E) fb(E) fb_notify(E) imx_sc_thermal(E) galcore(E) device_cooling(E) vehicle_rpmsg_m4(E)
 mux_mmio(E) trusty_virtio(E) trusty_ipc(E) trusty_log(E) trusty_irq(E) vehicle_core(E) imx_rpro
c(E) imx8_parallel_csi(CE) imx8_media_dev(CE) gmsl_max9286(CE) imx8_capture(CE) imx8_isi_capture
(CE) imx8_isi_mem2mem(CE)
[   56.460492][    C2]  imx8_isi_hw(CE) dwc_mipi_csi2(CE) imx8_mipi_csi2_sam(CE) imx8_mipi_csi2(
CE) timer_imx_sysctr(E) seco_mu(E) imx_dsp(E) sdhci_esdhc_imx(E) cqhci(E) imx_cpufreq_dt(E) cpuf
req_dt(E) imx_sc_wdt(E) amphion_vpu(E) mxc_mipi_csi2_yav(E) mxc_jpeg_encdec(E) v4l2_jpeg(E) ov56
40(E) v4l2_fwnode(E) v4l2_async(E) rtc_imx_sc(E) imx_sc_pwrkey(E) cdns3_imx(E) cdns3(E) cdns_usb
_common(E) gpio_switch(E) phy_mxs_usb(E) i2c_dev(E) i2c_mux_pca954x(E) i2c_mux(E) i2c_rpmsg_imx(
E) i2c_imx_lpi2c(E) dma_buf_imx(E) secure_heap(E) dsp_heap(E) cma_heap(E) system_heap(E) it6263(
E) nwl_dsi(E) mux_core(E) adv7511(E) cdns_mhdp_imx(E) cdns_mhdp_drmcore(E) imx_dcss(E) sec_mipi_
dsim_imx(E) sec_dsim(E) imx8qxp_ldb(E) imx8qm_ldb(E) fsl_imx_ldb(E) imx_ldb(E) arm_smmu_v3(E) ar
m_smmu(E) qcom_scm(E) fsl_lpuart(E) pf8x00_regulator(E) gpio_regulator(E) imx8m_pm_domains(E) bu
sfreq_imx8mq(E) mxs_dma(E) stmp_device(E) fsl_edma_v3(E) pwm_bl(E) pwm_imx27(E) nvmem_imx_ocotp_
scu(E) gpio_pca953x(E)
[   56.546562][    C2]  pinctrl_imx8qxp(E) pinctrl_imx8qm(E) pinctrl_scu(E) pinctrl_imx(E) phy_m
ixel_lvds_combo(E) phy_mixel_lvds(E) phy_fsl_samsung_hdmi(E) phy_fsl_imx8_mipi_dphy(E) phy_caden
ce_salvo(E) irq_imx_irqsteer(E) trusty_core(E) zsmalloc(E)
[   56.654032][    C2] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G         C OE     5.15.71-g279b46
e22312-dirty #14
[   56.663960][    C2] Hardware name: Freescale i.MX8QM MEK (DT)
[   56.669712][    C2] pstate: 804000c5 (Nzcv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   56.677382][    C2] pc : expire_timers+0xa8/0x1a0
[   56.682108][    C2] lr : __run_timers+0x180/0x1e4
[   56.686825][    C2] sp : ffffffc00a94bdf0
[   56.690839][    C2] x29: ffffffc00a94be00 x28: ffffffc00a853260 x27: ffffff8810303600
[   56.698692][    C2] x26: ffffffc00a66adf8 x25: ffffffc00a63d008 x24: dead000000000122
[   56.706546][    C2] x23: 0000000000000000 x22: ffffffc00a90d278 x21: 00000000ffff1200
[   56.714399][    C2] x20: ffffff88fcf6ef80 x19: ffffffc00a94be60 x18: ffffffc00a941038
[   56.722252][    C2] x17: ffffffc8f292f000 x16: 0000000000000000 x15: 0000000000000000
[   56.730106][    C2] x14: ffffffc00a90d278 x13: ffffff88fcf6f638 x12: 0000000000000040
[   56.737960][    C2] x11: ffffffc00a94be68 x10: ffffffffffffffff x9 : ffffffc00a94be60
[   56.745813][    C2] x8 : dead000000000122 x7 : 0000000000000001 x6 : fffffffdefb88a90
[   56.753667][    C2] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000200
[   56.761520][    C2] x2 : 0000000000000200 x1 : ffffffc00a94be60 x0 : ffffff88fcf6ef80
[   56.769384][    C2] Call trace:
[   56.772530][    C2]  expire_timers+0xa8/0x1a0
[   56.776897][    C2]  __run_timers+0x180/0x1e4
[   56.781267][    C2]  run_timer_softirq+0x28/0x58
[   56.785897][    C2]  _stext+0x134/0x4bc
[   56.789746][    C2]  __irq_exit_rcu.llvm.16159328691032069789+0x74/0x100
[   56.796461][    C2]  handle_domain_irq+0x80/0xf4
[   56.801092][    C2]  gic_handle_irq+0x54/0x114
[   56.805548][    C2]  call_on_irq_stack+0x3c/0x6c
[   56.810179][    C2]  do_interrupt_handler+0x44/0xa0
[   56.815070][    C2]  el1_interrupt+0x34/0x64
[   56.819353][    C2]  el1h_64_irq_handler+0x1c/0x2c
[   56.824157][    C2]  el1h_64_irq+0x7c/0x80
[   56.828266][    C2]  arch_local_irq_enable+0xc/0x18
[   56.833157][    C2]  default_idle_call+0x40/0x150
[   56.837875][    C2]  do_idle.llvm.13579087976232309098+0x100/0x2b8
[   56.844069][    C2]  cpu_startup_entry+0x28/0x2c
[   56.848699][    C2]  secondary_start_kernel+0x1ac/0x214
[   56.853938][    C2]  __secondary_switched+0x94/0x98
[   56.858836][    C2] Code: d503201f a94026c8 f9000128 b4000048 (f9000509) 
[   56.865633][    C2] ---[ end trace e36c04e90a71d350 ]---
[   56.894395][   T20] Kernel Offset: disabled
[   56.898583][   T20] CPU features: 0x2,00004163,20000846
[   56.903813][   T20] Memory Limit: none
[   56.907573][   T20] trusty-log trusty:trusty-log: panic notifier - trusty version Project: im
x8qm_a72, Build: build@pantakill-5, Built: 10:05:29 Nov  8 2022

U-Boot SPL 2022.04-g93f803c3-dirty (Jul 17 2023 - 09:15:59 +0800)
Normal Boot
Trying to boot from MMC1
Authentication key not yet programmed 
Booting from bootloader_a...
UU
  boot args 0x*** 0x*** 0x*** 0x0
initializing trusty (Project: imx8qm_a72, Build: build@pantakill-5, Built: 10:05:29 Nov  8 2022)
Core:  180 devices, 28 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0i2c: Error check busy bus: 0x8
it6263_i2c_reg_read, read err -102
faill to read from it6263 revision, ret -102
 (1280 x 720)
        [0] dpu@56180000, video
        [1] lvds-channel@0, display
        [2] lvds-to-hdmi-bridge@4c, video_bridge
In:    serial
Out:   serial
Err:   serial

 BuildInfo: 
  - SCFW 6638c032, SECO-FW c9de51c0, IMX-MKIMAGE d265bd1e, ATF 503f7fe
  - U-Boot 2022.04-g93f803c3-dirty 

flash target is MMC:0
Net:   eth0: ethernet@5b040000 [PRIME], eth1: ethernet@5b050000
INFO Initializing Trusty device
INFO selected trusty api version: 3 (requested 3)
INFO Initializing Trusty IPC device
INFO Initializing RPMB storage proxy service
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
failed to read rpmb write counter
Authentication key not yet programmed 
rpmb_proxy.c:279: ERROR proxy_handle_rpmb: rpmb_storage_send failed: 7
ss: block_device_tipc_init: bad static rpmb size, 2048
ss: proxy_connect: block_device_tipc_init failed (-1)
Authentication key not yet programmed 
INFO Initializing Trusty Hardware Crypto client
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
Verifying slot _a ...
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_validate_vbmeta_public_key_rpmb: Read public key error
avb_slot_verify.c:899: ERROR: vbmeta_a: Public key used to sign data rejected.
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
fsl_read_rollback_index_rpmb: read rollback from Trusty error!
Authentication key not yet programmed 
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
 verify FAIL, state: UNLOCK
 boot 'boot_a' still
Kernel load addr 0x80280000 size 21813 KiB
kernel   @ 80280000 (43253760)
ramdisk  @ fc000000 (19757977)
fdt      @ 82d40400 (138738)
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
ERROR - failed to read public key for keymaster
keymaster.c:318: ERROR Keymaster TIPC client not initialized!
keymaster.c:684: ERROR Keymaster TIPC client not initialized!
boota: set boot patch level failed.
avb.c:86: ERROR avb_do_tipc: AVB TIPC client not initialized
Authentication key not yet programmed 
Moving Image from 0x80280000 to 0x80400000, end=82d40000
## Flattened Device Tree blob at 82d40400
   Booting using the fdt blob at 0x82d40400
ERROR: reserving fdt memory region failed (addr=900ff000 size=1000 flags=4)
ERROR: reserving fdt memory region failed (addr=90400000 size=100000 flags=4)
ERROR: reserving fdt memory region failed (addr=90100000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90108000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90110000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=90118000 size=8000 flags=4)
ERROR: reserving fdt memory region failed (addr=901ff000 size=1000 flags=4)
ERROR: reserving fdt memory region failed (addr=91f00000 size=100000 flags=0)
   Using Device Tree in place at 0000000082d40400, end 0000000082d651f1

Starting kernel ...

[    0.000000][    T0] Booting Linux on physical CPU 0x0000000100 [0x410fd082]
[    0.000000][    T0] Linux version 5.15.71-g279b46e22312-dirty (bfz@bfz) (Android (8508608, ba
sed on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4
c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #14 SMP PREEMPT Mon Jul 17 09:33:11 CST 20
23
[    0.000000][    T0] Machine model: Freescale i.MX8QM MEK
[    0.000000][    T0] Stack Depot is disabled
[    0.000000][    T0] earlycon: lpuart32 at MMIO32 0x000000005a060000 (options '')
[    0.000000][    T0] printk: bootconsole [lpuart32] enabled
[    0.000000][    T0] efi: UEFI not found.
[    0.000000][    T0] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 Mi
B
[    0.000000][    T0] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-p
ool
[    0.000000][    T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 Mi
B
[    0.000000][    T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id sh
ared-dma-pool
[    0.000000][    T0] kvm [0]: Reserved 36 MiB at 0x97d000000
[    0.000000][    T0] Zone ranges:
[    0.000000][    T0]   DMA32    [mem 0x0000000080200000-0x00000000ffffffff]
[    0.000000][    T0]   Normal   [mem 0x0000000100000000-0x000000097fffffff]
[    0.000000][    T0] Movable zone start for each node
[    0.000000][    T0] Early memory node ranges
[    0.000000][    T0]   node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000084000000-0x00000000863fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000086400000-0x00000000887fffff]
[    0.000000][    T0]   node   0: [mem 0x000000008a800000-0x000000008fffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000090c00000-0x0000000091ffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092000000-0x00000000920fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092100000-0x00000000923fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000092400000-0x00000000951fffff]
[    0.000000][    T0]   node   0: [mem 0x0000000095200000-0x00000000fdffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000880000000-0x000000088fffffff]
[    0.000000][    T0]   node   0: [mem 0x0000000890000000-0x000000097fffffff]
[    0.000000][    T0] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff]
[    0.000000][    T0] On node 0, zone DMA32: 512 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone DMA32: 8192 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone DMA32: 3072 pages in unavailable ranges
[    0.000000][    T0] On node 0, zone Normal: 8192 pages in unavailable ranges
[    0.000000][    T0] cma: Reserved 928 MiB at 0x00000000c2000000
[    0.000000][    T0] psci: probing for conduit method from DT.
[    0.000000][    T0] psci: PSCIv1.1 detected in firmware.
[    0.000000][    T0] psci: Using standard PSCI v0.2 function IDs
[    0.000000][    T0] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000][    T0] psci: SMC Calling Convention v1.2
[    0.000000][    T0] Load bootconfig: 1018 bytes 64 nodes
[    0.000000][    T0] percpu: Embedded 29 pages/cpu s81752 r8192 d28840 u118784
[    0.000000][    T0] Detected PIPT I-cache on CPU0
[    0.000000][    T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[    0.000000][    T0] CPU features: detected: GIC system register CPU interface
[    0.000000][    T0] CPU features: detected: Spectre-v2
[    0.000000][    T0] CPU features: detected: Spectre-v3a
[    0.000000][    T0] CPU features: detected: Spectre-BHB
[    0.000000][    T0] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000][    T0] Built 1 zonelists, mobility grouping on.  Total pages: 1528328
[    0.000000][    T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.
mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init firmware_class.
path=/vendor/firmware loop.max_part=7 bootconfig cma=928M@0x960M-0xfc0M transparent_hugepage=nev
er moal.mod_para=wifi_mod_para.conf pci=nomsi video=HDMI-A-2:d bootconfig buildvariant=userdebug
[    0.000000][    T0] cgroup: Disabling pressure control group feature
[    0.000000][    T0] Unknown kernel command line parameters "buildvariant=userdebug", will be 
passed to user space.
[    0.000000][    T0] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linea
r)
[    0.000000][    T0] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000][    T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[    0.000000][    T0] software IO TLB: mapped [mem 0x00000000be000000-0x00000000c2000000] (64MB
)
[    0.000000][    T0] Memory: 4624248K/6211584K available (18496K kernel code, 2262K rwdata, 19
172K rodata, 1472K init, 613K bss, 637064K reserved, 950272K cma-reserved)
[    0.000000][    T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1
[    0.000000][    T0] trace event string verifier disabled
[    0.000000][    T0] rcu: Preemptible hierarchical RCU implementation.
[    0.000000][    T0] rcu:     RCU event tracing is enabled.
[    0.000000][    T0] rcu:     RCU dyntick-idle grace-period acceleration is enabled.
[    0.000000][    T0] rcu:     RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=6.
[    0.000000][    T0] rcu:     RCU priority boosting: priority 1 delay 500 ms.
[    0.000000][    T0]  Trampoline variant of Tasks RCU enabled.
[    0.000000][    T0]  Tracing variant of Tasks RCU enabled.
[    0.000000][    T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000][    T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6
[    0.000000][    T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000][    T0] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000][    T0] GICv3: 512 SPIs implemented
[    0.000000][    T0] GICv3: 0 Extended SPIs implemented
[    0.000000][    T0] GICv3: Distributor has no Range Selector support
[    0.000000][    T0] Root IRQ handler: gic_handle_irq.0063cfc43c850c778600e9fd9282e821.cfi_jt
[    0.000000][    T0] GICv3: 16 PPIs implemented
[    0.000000][    T0] GICv3: CPU0: found redistributor 100 region 0:0x0000000051b80000
[    0.000000][    T0] ITS: No ITS available, not enabling LPIs
[    0.000000][    T0] rcu:     Offload RCU callbacks from CPUs: (none).
[    0.000000][    T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval_
___)-0x(____ptrval____)
[    0.000000][    T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000][    T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854
df40, max_idle_ns: 440795202120 ns
[    0.000000][    T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500
ns
[    0.009339][    T0] Calibrating delay loop (skipped), value calculated using timer frequency.
. 16.00 BogoMIPS (lpj=32000)
[    0.019957][    T0] pid_max: default: 32768 minimum: 301
[    0.025423][    T0] LSM: Security Framework initializing
[    0.030603][    T0] SELinux:  Initializing.
[    0.034950][    T0] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.043020][    T0] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linea
r)
[    0.053435][    T1] rcu: Hierarchical SRCU implementation.
[    0.059252][    T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build
[    0.067755][    T1] EFI services will not be available.
[    0.073102][    T1] smp: Bringing up secondary CPUs ...
[    0.079238][    T0] Detected PIPT I-cache on CPU1
[    0.079273][    T0] GICv3: CPU1: found redistributor 101 region 0:0x0000000051ba0000
[    0.079307][    T0] CPU1: Booted secondary processor 0x0000000101 [0x410fd082]
[    0.081640][    T0] CPU features: detected: ARM erratum 845719
[    0.081659][    T0] Detected VIPT I-cache on CPU2
[    0.081694][    T0] GICv3: CPU2: found redistributor 0 region 0:0x0000000051b00000
[    0.081747][    T0] CPU2: Booted secondary processor 0x0000000000 [0x410fd034]
[   21.104265][    C0] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[   21.155629][    C0] rcu:     2-O...: (0 ticks this GP) idle=001/1/0x4000000000000004 softirq=
0/0 fqs=2625 last_accelerate: 0000/ef98 dyntick_enabled: 0
[   21.168916][    C0]  (detected by 0, t=5252 jiffies, g=-1195, q=2)
[   21.175084][    C0] rcu: Offline CPU 2 blocking current GP.
[   84.243587][    C0] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[   84.250027][    C0] rcu:     2-O...: (0 ticks this GP) idle=001/1/0x4000000000000004 softirq=
0/0 fqs=10503 last_accelerate: 0000/2d23 dyntick_enabled: 0
[   84.263405][    C0]  (detected by 0, t=21007 jiffies, g=-1195, q=2)
[   84.269659][    C0] rcu: Offline CPU 2 blocking current GP.
This is my boot log
0 Kudos
Reply
1 Reply

2,145 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using? Which version of BSP are you using? Please double check the dtb file that you are loading in the u-boot. 

0 Kudos
Reply