大家好:
1. i.MX8QM Linux内核针对Xen dts示例中有fsl-imx8qm-mek-dom0.dts、fsl-imx8qm-mek-domu.dts;
2. 在示例中,Dom0运行Linux并使用dpu1, Domu运行Android并使用dpu2;
3. 是否可以做到让Domu使用dpu2运行Linux、Dom0使用dpu1运行Android?主要是因为我们想给Android使用HDMI;
4. 在哪里可以获取到一些参考?
谢谢
---------------------------------------------------------------------------------------------------------------------------------
Hi All:
1. There are fsl-imx8qm-mek-dom0.dts/fsl-imx8qm-mek-domu.dts in i.MX8QM Linux kernel for Xen dts example;
2. Dom0 run Linux with dpu1 and Domu run Android with dpu2 with the example;
3. Can i use dpu1 for domu to run Android and dpu2 for dom0 to run Linux? i just want to use HDMI for Android;
4. How can I get a reference?
Thanks at first.
I only find dual linux sample for this, because imx8 is under preproduction, so we don't have enough information to share, if you need more detailed information, pls contact professinoal service: