Hi
I want to use L4.19.35 bsp to compile i.MX8QM image. And the ddr should be modify. So download SCFW source code about imx-scfw-porting-kit-1.2.7.1 , but when I download RPA , the older version is V20, but it will cause some compile error aboult RDBI_bit_deskew(0); function can not find.
Can you send me the MX8QM_B0_LPDDR4_RPA_1.6GHz_v17.xlsx ?
已解决! 转到解答。