i.MX8QM RPA_V17 request

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM RPA_V17 request

Jump to solution
920 Views
coindu
Contributor IV

Hi

           I want to use L4.19.35 bsp to compile i.MX8QM image. And  the ddr should be modify. So download SCFW source code about imx-scfw-porting-kit-1.2.7.1 , but when I download RPA , the older version is V20, but it will cause some compile error aboult RDBI_bit_deskew(0); function can not find.

 

         Can you send me the MX8QM_B0_LPDDR4_RPA_1.6GHz_v17.xlsx ?

0 Kudos
Reply
1 Solution
912 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello coindu.

Please find attached file.

 

Best regards

Harvey

View solution in original post

0 Kudos
Reply
1 Reply
913 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello coindu.

Please find attached file.

 

Best regards

Harvey

0 Kudos
Reply