Hi all,
I want to set up a Wifi connection on the i.MX8QM MEK with the EAR00315 wifi module. How can I check that the module is connected to the board correctly? Which kind of configuration is required? Do any specific driver exist for QNX? Unfortunately there is no manual existing on how to start.
Thanks a lot.
Hi ,
Probably 2 ways you can try.
---Asking QNX company for help, comfiring if they can provide EAR00315 wifi driverf for QNX, because they QNX bsp is designed by them.
---Poring EAR00315 wifi for linux to QNX platform.
we only provide customer linux and android bsp.
Hope above messages are helpful to you.
Have a nice day!
B.R,
weidong
One step further, I use the "io-pkt-v6-hc -d mx8xp ..." command to configure the Ethernet network with the BSP provided. How can I establish a wifi connection?