i.MX8QM: How Cortex-M4 access another cores' LPUART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM: How Cortex-M4 access another cores' LPUART

1,225 Views
michaeltang_ltc
Contributor II

Hello there,

I'm wondering if it's possible to access each cores' LPUART, said, CM4_0 access CM4_1's LPUART? How to capture/send the message in another core?

I found the base address of M4_0__LPUART and M4_1__LPUART is different, in MIMX8QM6_cm4_core0.h,

  • #define CM4_0__LPUART_BASE (0x41220000u)
  • #define CM4_1__LPUART_BASE (0x3B220000u)

and in MIMX8QM6_cm4_core1.h, it is

  • #define CM4_0__LPUART_BASE (0x37220000u)
  • #define CM4_1__LPUART_BASE (0x41220000u)

, but the IRQ number is the same:

  • M4_0_LPUART_IRQn = 25
  • M4_1_LPUART_IRQn = 25

I though it's possible to access each others UART but the interrupt might be a problem.

pastedImage_2.png

0 Kudos
4 Replies

1,097 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

such access is performed using "partition" concept, please check relevant

documentation and SCU APIs on:

System Controller Firmware 101 - Resource management service 

SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,097 Views
michaeltang_ltc
Contributor II

Hi Igor,

Thanks for your reply, I thought the SCFW resource partitioning mechanism is providing an access guard for different resources. But how about the M4_x_LPUART_IRQn? They're in the same number in each core. Does the INTMUX of CM4 is used for passing interrupt from CM4_0 to CM4_1? Do you have any suggestion for cross-core-handling of the dedicated interrupt?

Best regards,

Michael Tang

0 Kudos

964 Views
vinothkumars
Senior Contributor IV

Hi @michaeltang_ltc 

 

Did you find the solution ?

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos

1,097 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

for M4 please look at examples in SDK_MIMX8QM_M4

Welcome | MCUXpresso SDK Builder 

Best regards
igor

0 Kudos