i.MX8QM Camera commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8QM Camera commands

1,410件の閲覧回数
prashanthkumar
Contributor II

Hi,

 

Can u provide me the gst commands for i.MX8QM MIPI OV5640 camera overlay and capture?

Using imx-yocto-L4.14.78_1.0.0_ga release.

 

Thanks and Regards,

Prashanth Kumar K

0 件の賞賛
返信
2 返答(返信)

1,151件の閲覧回数
s233199
Contributor II

Hi, you are using an IMX8 QM board with imx-yocto-L4.14.78_1.0.0_ga release, right? I am trying to boot an image on my IMX8qmlpddr4arm2 board with sumo but this image can't boot. I have reproduced the steps on the yocto manual but I do not know why it fails Did you have this kind of problems?

Sorry for this out of topic question but I have not found informations that could help me yet.

Thank you, and sorry for bad english.

Erica

0 件の賞賛
返信

1,151件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth

one can check Linux L4.14.78_1.0.0 Documentation

Table 16. i.MX GStreamer 1.0 plugins Release Notes shows supported

plugins for each family, according to it :

i.MX 8 Family: • v4l2src: V4L2-based camera source plugin

Sect.7.3.8 Camera preview Linux Guide describes plugins usage.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信