i.MX8Q suspend pin settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8Q suspend pin settings

1,405 Views
Maddis
Contributor IV

Hi,

 

We have i.MX8DX(actually atm. we use i.MX8Q) based HW that has our own System Supervisor - processor and the i.MX8. We have two GPIO-pins that we use to signal to our System Supervisor if i.MX8 wants to shutdown or reboot. Then of course there is the PMIC Standby - signal that indicates if i.MX8 wants to go suspend - mode. Those two GPIO-pins have pull-down/up - resistors to pull them to known state for startup.

 

Problem now is that when entering suspend mode from Linux the i.MX8 puts those two GPIO-pins in hi-z - mode(I measured with oscilloscope and verified from waveform that pin is actually floating and signals are not being driven to that wrong mode) and they’ll get pulled to wrong state causing System Supervisor actually reboot the system instead suspend. Suspend request is sent after that, but it’s too late.

 

I found in pad/mux - control register these settings:

 

lower power configuration

00b - PASS

01b - EARLY_ISO

10b - LATE_ISO

11b - LATCH

 

I’ve tried them, but seems that they don’t have any affect. I looked through the manual, but couldn’t figure out how can I keep the drive on even when the i.MX8 enters to low power mode?

 

Pins in question are:

 

SAI0_TXFS_LSIO_GPIO0_IO28

SAI1_RXD_LSIO_GPIO0_IO29

 

We are using if not latest then quite recent BSP for i.MX8 and kernel 4.19.35.

0 Kudos
5 Replies

1,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi mc

this was observed in early silicon/bsp revisions however fixed later.

Suggest to try with latest i.MX8X C0 silicon and linux Linux 4.14.98_2.3.0

Linux 4.14.98_2.3.0 Documentation

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,215 Views
Maddis
Contributor IV

Hi,

Thanks for the confirmation that it's/was known issue.

Seems that this is the issue since we have B0 silicon, but we are already using kernel 4.19.35 from (https://source.codeaurora.org/external/imx/meta-fsl-bsp-release branch: warrior-4.19.35-1.1.0 )

Do you know if that should also have the suspend patch or is it only in that 4.14 -kernel?

Another question is that should we use those separate kernel repositories or use kernel that comes with each BSP? Seems that using directly those kernel repositories we might get more recent kernel than what comes with BSP.

0 Kudos

1,215 Views
igorpadykov
NXP Employee
NXP Employee

for i.MX8X recommended to use exactly L4.14.98_2.3.0 (not 4.19.35) and

production rev.C0 silicon (marking starting with "M", ending "AC").

linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos

1,215 Views
Maddis
Contributor IV

Well this is interesting. 

Latest BSP (that we were told to use by NXP) doesn't even contain 4.14 - kernel. Only 4.19.35.

Looking at this: meta-fsl-bsp-release - i.MX Yocto Project Release Layer 

The 'latest' is warrior-4.19.35-1.1.0. Last change is done to sumo-4.14.98-2.3.0, but sumo is already almost two years old so doesn't really qualify as 'latest'.  But if you say 4.14.98_2.3.0 should be used we'll investigate that then. But we also have too old silicon atm. too.

0 Kudos

1,215 Views
igorpadykov
NXP Employee
NXP Employee

Linux L4.14.98_2.3.0 ,  official nxp linux  source.codeaurora.org/external/imx/linux-imx  repository

linux-imx - i.MX Linux kernel 

Linux 4.14.98_2.3.0 Documentation

0 Kudos