i.MX8Q Android How to enable WM8960 output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8Q Android How to enable WM8960 output

ソリューションへジャンプ
2,944件の閲覧回数
n3820fjmn2k2q
Contributor I

I'm using i.MX8QXP MEK CORE&BaseBoard. This board has 2 codec, CS42888 and WM8960.

As default, CS42888 output is enabled. But I wanna use WM8960 in CORE board.

What do I do in order to change audio-routing? Or... I wanna to know the way enable both codec.

Regards,

Kikuchi

ラベル(2)
0 件の賞賛
返信
1 解決策
2,493件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Makotonosuke

one can try to enable (set status = "okay") wm8960 in dts file:

linux/arch/arm64/boot/dts/freescale/fsl-imx8qxp-mek.dts

fsl-imx8qxp-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,494件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Makotonosuke

one can try to enable (set status = "okay") wm8960 in dts file:

linux/arch/arm64/boot/dts/freescale/fsl-imx8qxp-mek.dts

fsl-imx8qxp-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,493件の閲覧回数
n3820fjmn2k2q
Contributor I

Hi igor.

Now, I set WM8960 "okay" in dts, and CS42888 "disabled".

Then, WM's Headphone port is active!

Thanks a lot!

0 件の賞賛
返信