i.MX8MQ6CVAHZAA Cold Test USB 3.0 Enumeration issue below 0°C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ6CVAHZAA Cold Test USB 3.0 Enumeration issue below 0°C

2,359 Views
nilavchoksi
Contributor III

Hi NXP Team,

We have designed i.MX8MQ6 based boards with maximum available interfaces and currently we are in the Design validation and testing phase.

Boards are working as expected in the Normal Condition.

Currently, we are working on Thermal Testing and found enumeration issue during cold Tests below 0C. When we put the device in the chamber below 0 degrees or do a cold spray on the board, USB3.0 superspeed device not able to enumerate however USB2.0 device can detect properly on the same port.

We have added a power switch with USB3.0 which is the same as per USB2.0. and common mode code as per attached USB3.0 Interface circuit.

Kindly share your suggestions/feedback.

Thank you,

Nilav Choksi. 

Labels (1)
0 Kudos
Reply
3 Replies

2,293 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Nilav Choksi,

Have you test above 0 degree? Does it work well?

Best Regards

Rita

0 Kudos
Reply

2,293 Views
nilavchoksi
Contributor III

Hi Rita Wang,

Yes, we have tested above 0 Degree and it is working Well. But during Cold Test USB3.0 super peed is failing during Enumeration and another USB2.0 interface is working fine.

Both the different interfaces supported in the processor have the same components in between processor pin to connector pins.

Thank you,

Nilav Choksi

0 Kudos
Reply

2,293 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Nilav Choksi,

I will confirm it for you. Then update to you.

Have a nice day

Rita

0 Kudos
Reply