Hello,
Release: Yocto-Sumo (4.14.78_1.0.0_GA)
Board: i.MX8MQ based custom board
I want to change the debug console from UART1 to UART3 on iMX8MQ based board. I have updated header, source and dts files at U-boot source and did necessary changes in the kernel sources. But, I was not able to get data over other UART3 port.
I have attached a patch that I applied to the U-boot source.
Is anything I am missing to do that? If any working solution is available then provide the same.
Thanks and regards,
Nirmal