i.MX8MQ and LPDDR4 with 800MHz + 200MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ and LPDDR4 with 800MHz + 200MHz

Jump to solution
1,086 Views
christian_mauderer
Contributor III

Hello,

we have a custom board with an MIMX8MQ5DVA with mask set 0N14W. We use that together with a Samsung K4F8E3S4HB-MFCJ LPDDR4. The RAM is running with 800MHz as main frequency and 200MHz for the FREQ1 set point.

The first prototypes of the board worked well and so we started production. Now we have quite some boards where the RAM training fails during U-Boot SPL (about 5 to 10 %) on some boards with a temperature dependency. If I try to train these boards with the "NXP i.MX/Mscale DDR Tool" Version 2.10 for 800MHz and 200MHz I get a fail with the output at the end of the post. The same is true for Version 1.0 that we originally used for the boards. The odd thin is: 800MHz + 334MHz work fine.

My colleague found the erratum e11327 "DDR PHY: LPDDR4 may fail when switching from PHY PLL bypass mode to
PHY PLL Mission mode" for our mask set:

i.MX8M e11327.png

Is it likely that the behavior we see is connected to the erratum? Is there some workarround for it except for using 334MHz? We would really like to get the extra energy saving of the 200MHz.

With kind regards

Christian Mauderer

DDR Tool output with 800MHz + 200MHz:

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @800Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @200Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @800Mhz...
[Process] End of initialization
PMU: Error: No passing region found for 1 or more lanes. Set hdtCtrl=4 to see passing regions
PMU: ***** Assertion Error - terminating *****
[Result] FAILED
Labels (1)
0 Kudos
Reply
1 Solution
855 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian 

>Is it likely that the behavior we see is connected to the erratum?

yes this is correct.

>Is there some workarround for it except for using 334MHz?

sorry no workaround is available, recommended to use latest revision where it is fixed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
856 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian 

>Is it likely that the behavior we see is connected to the erratum?

yes this is correct.

>Is there some workarround for it except for using 334MHz?

sorry no workaround is available, recommended to use latest revision where it is fixed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply