i.MX8MQ EVK cannot boot from SD card and eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MQ EVK cannot boot from SD card and eMMC

3,042件の閲覧回数
Derek0902
Contributor II

Hi,

I use the customized board and the Linux version is 6.1.36-2.1.0. Then I use core-image-minimal as boot image. When the board is booting up, it cannot enter kernel  and stop at this log.

SD card :

SDcard.png

eMMC :

emmcboot_minimal.png

The attached file is the complete log of booting from eMMC.

 

Can anyone provide the correct boot log?

 

Thanks & Regards,

Derek Lin

0 件の賞賛
返信
4 返答(返信)

3,022件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Derek0902 

Please find the attachment for both boot log of SD and eMMC.

 

Regards

Harvey

0 件の賞賛
返信

3,018件の閲覧回数
Derek0902
Contributor II

Hi @Harvey021 ,

Thanks for your help!

I have a question that is possible to decrease CPU frequency in u-boot? Is it possible to solve the boot problem?

Cpufreq.png

 

Thanks & Regards,

Derek Lin

0 件の賞賛
返信

2,961件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Can't see boot problem from the CPU Freq. About decreasing Freq, you can have a try to modify "int clock_init" from clock_imx8mq.c in uboot.

 

Regards

Harvey

0 件の賞賛
返信

2,932件の閲覧回数
Derek0902
Contributor II

Hi @Harvey021 ,

I found that it only support two grades. Can it be modified lower frequency than 800MHz?

Derek0902_0-1702439562577.png

 

And I have disabled almost all the device that I don't need or unusual. It stop at "waiting for root device". The roofs doesn't be mounted.  I think that It doesn't seem to be related to CPU frequency. What could be the problem?

quad.png

 

Regards,

Derek Lin

0 件の賞賛
返信