i.MX8MPlus Windows 10 IoT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MPlus Windows 10 IoT

Jump to solution
2,022 Views
leven
Contributor I

We use i.MX8MPlus to run Windows 10 IoT system and encounter the compatibility problem of Samsung eMMC. How to solve it? Details are as follows:

1. Failed to run Windows 10 IoT using Samsung /KLMAG1JETD-B041/16GB eMMC5.1

2. Windows 10 IoT was successfully run with Samsung /KLMAG2GEUF-B04P/16GB eMMC5.1.

3. The above two Samsung eMMC burning ubuntu system runs normally, but there is a difference in running Wingdows 10 IoT.

4. The picture shows the comparison between operation failure and success.Windows OK vs  NG.png

Labels (1)
0 Kudos
Reply
1 Solution
2,015 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

View solution in original post

0 Kudos
Reply
5 Replies
1,949 Views
anthonychen-msft
Contributor II

Do you have the datasheets for the two Samsung parts? I'm curious what their differences might be.

Also do you have the whole video showing where the script actually fails?

0 Kudos
Reply
2,004 Views
leven
Contributor I

Hi Bio_TICFSL:

We ran Windows 10 IoT with the new Samsung /KLMAG1JETD-B041/16GB chip and still failed.

We erased the Samsung /KLMAG1JETD-B041/16GB chip and still failed to run Windows 10 IoT.

Running the following command to erase also fails : 

# destroy the partition table

dd if=/dev/zero of=/dev/sdx bs=1024 count=1

0 Kudos
Reply
1,605 Views
mirkoardinghi1
Contributor IV

I have the same problem, Do you find a solution?

0 Kudos
Reply
842 Views
aber
Contributor III

By default, it only supports emmc above 32g. 

0 Kudos
Reply
2,016 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

0 Kudos
Reply