Hi all, I'm working through a design and wanted to get some clarification on the USB ports on the iMX8M PLUS mcu. I see that it has 4 separate PHYs, two USB2 and 2 USB3. Can those ports be used completely separately? As in, can I connect two USB 2 devices and 2 USB 3 devices (for a total of four different devices) at once? Additionally, do the paired USB 2.0/3.0 PHYs share bandwidth in any internal upstream interface? If I saturate USB 3.0 port 1, could I end up starving USB 2.0 port 1 of bandwidth?
Thank you