i.MX8MP FEC Controller interfaced with KSZ9477 - TX Clock Variation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MP FEC Controller interfaced with KSZ9477 - TX Clock Variation

1,077 Views
shivani__p
Contributor II

Hi,

We have used KSZ9477 chip on our i.MX8M Plus platform based custom board.
We have interfaced KSZ9477 with FEC (freescale) MAC through RGMII.

We have integrated the driver for KSZ9477 switch from
https://github.com/Microchip-Ethernet/EVB-KSZ9477/tree/master/KSZ/linux-drivers/ksz9897/linux-5.3/dr... for micrel and Freescale.

By default, KSZ9477 chip is configured to 1gbps speed. And we are able to ping the device when the link speed is 1gbps.
But we are not able to ping when the link speed changes to 100mbps. In this scenario, we observed that
for 1 gbps speed, RX clock is 125 MHz and TX Clock is 125 MHz.
But for 100mbps, the RX Clock is 125MHz but TX Clock chnages to 25 MHz.

Due to this ping doesn't work.

For this to work, we have to change the KSZ9477 speed to 100 mbps.

So, it seems to be issue with FEC controller which is not able to set the TX clock to fixed 125MHz.
We have not observed this behaviour with STMMAC Controller interfaced to KSZ9897 on i.MX8MP.
and also with FEC Controller in i.MX6sx interfaced to KSZ9477.

Can you please help with this?

 

Thanks,

Shivani Patel

Labels (1)
0 Kudos
Reply
1 Reply

1,067 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shivani

 

one can try latest nxp linux 5.10.52_2.1.0, it has ksz9477 driver

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/net/dsa/microchip/ksz9477.c?h=lf-5...

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

>.. it seems to be issue with FEC controller which is not able to set the TX clock to fixed 125MHz.

 

if issue in fec driver, it should be reproducable on i.MX8M Plus EVK, please provide steps how

it can be reproduced for help to analyze it on nxp side.

 

Best regards
igor

0 Kudos
Reply