i.MX8MMini FlexSPI can't boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MMini FlexSPI can't boot issue

1,040 Views
Danube
Contributor IV

Hi ,

We use default L4.14.78 default flexspi image to program i.MX8Mmini EVK (Rev C) by uuu tool

we see console log is show OK.

But We change to flexspi boot , it can't boot and console can't out any debug log.

Is default flexspi image correct ?

EVK console log

SF: Detected n25q256a with page size 256 Bytes, erase size 4 KiB, total 32 MiB
Detect USB boot. Will enter fastboot mode!
SF: 1048576 bytes @ 0x0 Erased: OK
Detect USB boot. Will enter fastboot mode!
Detect USB boot. Will enter fastboot mode!
Starting download of 1434984 bytes
..........
downloading of 1434984 bytes finished
device 0 offset 0x15e568, size 0x1ea1a98
SF: 32119448 bytes @ 0x15e568 Written: OK

Windows uuu command console

D:\MFG_8mm_Linux>uuu.exe uuu_spinor_8mm.uuu
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.91-0-g3799f4d

Success 1    Failure 0

1:3    6/ 6   [Done                        ] FB: done

My uuu for flexspi boot setting

--> See uuu_spinor_8mm.uuu

0 Kudos
Reply
1 Reply

866 Views
igorpadykov
NXP Employee
NXP Employee

Hi Apollo

one can try procedure given in sect.7.3 Run an example application [5]

attached Getting Started with MCUXpresso SDK for i.MX 8M Mini.pdf,

replace uboot with imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi.

Also one can try with L4.14.98 images

Linux Binary Demo Files - i.MX 8MMini EVK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply