hello,
i am trying to do the M4 wakeup A53 part.
I understand that there is a patch needed to acheive this as per https://community.nxp.com/docs/DOC-343113 But i am on 5.4.24 kernel on my imx8mm, so looks like there are many changes and i dont see any irq/isr code there under imx_rpmsg.c. Any help is appreciated to figure out how this can be enabled on 5.4 kernel.
Hi Siva
I am afraid such patch is not available for i.MX8M Mini, also it has very different design
compared with i.MX8QXP processor. As starting point one can look at AN12195
Implement Low-Power Audio on i.MX8M
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------