i.MX8MM: M4 wake up A53 through RPMsg on kernel 5.4.24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM: M4 wake up A53 through RPMsg on kernel 5.4.24

646 Views
siva_prabhakara
Contributor III

hello, 

i am trying to do the M4 wakeup A53 part.

I understand that there is a patch needed to acheive this as per https://community.nxp.com/docs/DOC-343113  But i am on 5.4.24 kernel on my imx8mm, so looks like there are many changes and i dont see any irq/isr code there under imx_rpmsg.c. Any help is appreciated to figure out how this can be enabled on 5.4 kernel.

0 Kudos
1 Reply

608 Views
igorpadykov
NXP Employee
NXP Employee

Hi Siva

I am afraid such patch is not available for i.MX8M Mini, also it has very different design

compared with i.MX8QXP processor. As starting point one can look at AN12195

Implement Low-Power Audio on i.MX8M

AN12195SW.zip

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos