Hi,
we have a custom board with i.MX8M-Mini and ethernet PHY Microsemi VSC8531 connected via RGMII. While the interface works fine in general for link speeds of 10, 100 and 1000 MBit/s, there's an issue with the bandwith sometimes dropping to 50% of the expected/nominal value.
This issue can be seen with link speeds of 100 or 1000 MBit/s. In both cases the TX bandwidth is sometimes as expected (~93 MBit/s for link speed 100, ~900 MBit/s for link speed 1000) and sometimes it drops to much lower values like in the examples below (~45 MBit/s for link speed 100, ~600 MBit/s for link speed 1000).
The same behavior can be seen using a simple test with netcat, so it's not an iperf issue.
Looking at the statistics of the interface in Linux, there's nothing conspicuous. No packets are dropped and no errors reported.
So far we have tested and reproduced this behavior with Linux Kernel 5.4 and 5.10.
If anyone has any idea of what might be the cause of this, that would be great!
Thanks for your help!
Frieder
root@kontron-mx8mm:~# iperf3 -c 192.168.1.10 --bidir
Connecting to host 192.168.1.10, port 5201
[ 5] local 192.168.1.20 port 53574 connected to 192.168.1.10 port 5201
[ 7] local 192.168.1.20 port 53576 connected to 192.168.1.10 port 5201
[ ID][Role] Interval Transfer Bitrate Retr Cwnd
[ 5][TX-C] 0.00-1.00 sec 5.79 MBytes 48.6 Mbits/sec 0 80.6 KBytes
[ 7][RX-C] 0.00-1.00 sec 10.9 MBytes 91.8 Mbits/sec
[ 5][TX-C] 1.00-2.00 sec 5.28 MBytes 44.3 Mbits/sec 0 89.1 KBytes
[ 7][RX-C] 1.00-2.00 sec 11.1 MBytes 92.9 Mbits/sec
[ 5][TX-C] 2.00-3.00 sec 5.34 MBytes 44.8 Mbits/sec 0 93.3 KBytes
[ 7][RX-C] 2.00-3.00 sec 11.1 MBytes 92.8 Mbits/sec
[ 5][TX-C] 3.00-4.00 sec 5.16 MBytes 43.3 Mbits/sec 0 93.3 KBytes
[ 7][RX-C] 3.00-4.00 sec 11.1 MBytes 92.9 Mbits/sec
[ 5][TX-C] 4.00-5.00 sec 5.34 MBytes 44.8 Mbits/sec 0 93.3 KBytes
[ 7][RX-C] 4.00-5.00 sec 11.1 MBytes 92.8 Mbits/sec
[ 5][TX-C] 5.00-6.00 sec 5.41 MBytes 45.4 Mbits/sec 0 93.3 KBytes
[ 7][RX-C] 5.00-6.00 sec 11.1 MBytes 92.9 Mbits/sec
[ 5][TX-C] 6.00-7.00 sec 5.53 MBytes 46.4 Mbits/sec 0 130 KBytes
[ 7][RX-C] 6.00-7.00 sec 11.1 MBytes 92.8 Mbits/sec
[ 5][TX-C] 7.00-8.00 sec 5.28 MBytes 44.3 Mbits/sec 0 130 KBytes
[ 7][RX-C] 7.00-8.00 sec 11.1 MBytes 92.8 Mbits/sec
[ 5][TX-C] 8.00-9.00 sec 5.28 MBytes 44.3 Mbits/sec 0 130 KBytes
[ 7][RX-C] 8.00-9.00 sec 11.1 MBytes 92.8 Mbits/sec
[ 5][TX-C] 9.00-10.00 sec 5.28 MBytes 44.3 Mbits/sec 0 130 KBytes
[ 7][RX-C] 9.00-10.00 sec 11.1 MBytes 92.9 Mbits/sec
- - - - - - - - - - - - - - - - - - - - - - - - -
[ ID][Role] Interval Transfer Bitrate Retr
[ 5][TX-C] 0.00-10.00 sec 53.7 MBytes 45.0 Mbits/sec 0 sender
[ 5][TX-C] 0.00-10.01 sec 53.2 MBytes 44.6 Mbits/sec receiver
[ 7][RX-C] 0.00-10.00 sec 112 MBytes 94.1 Mbits/sec 0 sender
[ 7][RX-C] 0.00-10.01 sec 111 MBytes 92.7 Mbits/sec receiver
iperf Done.
root@kontron-mx8mm:~# iperf3 -c 192.168.1.10 --bidir
Connecting to host 192.168.1.10, port 5201
[ 5] local 192.168.1.20 port 53568 connected to 192.168.1.10 port 5201
[ 7] local 192.168.1.20 port 53570 connected to 192.168.1.10 port 5201
[ ID][Role] Interval Transfer Bitrate Retr Cwnd
[ 5][TX-C] 0.00-1.00 sec 74.4 MBytes 624 Mbits/sec 2 438 KBytes
[ 7][RX-C] 0.00-1.00 sec 106 MBytes 885 Mbits/sec
[ 5][TX-C] 1.00-2.00 sec 70.5 MBytes 591 Mbits/sec 24 321 KBytes
[ 7][RX-C] 1.00-2.00 sec 108 MBytes 905 Mbits/sec
[ 5][TX-C] 2.00-3.00 sec 69.3 MBytes 582 Mbits/sec 0 389 KBytes
[ 7][RX-C] 2.00-3.00 sec 107 MBytes 895 Mbits/sec
[ 5][TX-C] 3.00-4.00 sec 74.2 MBytes 622 Mbits/sec 14 385 KBytes
[ 7][RX-C] 3.00-4.00 sec 108 MBytes 906 Mbits/sec
[ 5][TX-C] 4.00-5.00 sec 69.2 MBytes 581 Mbits/sec 0 434 KBytes
[ 7][RX-C] 4.00-5.00 sec 107 MBytes 897 Mbits/sec
[ 5][TX-C] 5.00-6.00 sec 70.3 MBytes 590 Mbits/sec 14 191 KBytes
[ 7][RX-C] 5.00-6.00 sec 108 MBytes 902 Mbits/sec
[ 5][TX-C] 6.00-7.00 sec 68.0 MBytes 571 Mbits/sec 0 354 KBytes
[ 7][RX-C] 6.00-7.00 sec 107 MBytes 900 Mbits/sec
[ 5][TX-C] 7.00-8.00 sec 73.9 MBytes 620 Mbits/sec 1 356 KBytes
[ 7][RX-C] 7.00-8.00 sec 106 MBytes 892 Mbits/sec
[ 5][TX-C] 8.00-9.00 sec 72.9 MBytes 611 Mbits/sec 2 310 KBytes
[ 7][RX-C] 8.00-9.00 sec 108 MBytes 905 Mbits/sec
[ 5][TX-C] 9.00-10.00 sec 74.4 MBytes 624 Mbits/sec 0 404 KBytes
[ 7][RX-C] 9.00-10.00 sec 108 MBytes 903 Mbits/sec
- - - - - - - - - - - - - - - - - - - - - - - - -
[ ID][Role] Interval Transfer Bitrate Retr
[ 5][TX-C] 0.00-10.00 sec 717 MBytes 602 Mbits/sec 57 sender
[ 5][TX-C] 0.00-10.00 sec 715 MBytes 599 Mbits/sec receiver
[ 7][RX-C] 0.00-10.00 sec 1.05 GBytes 901 Mbits/sec 0 sender
[ 7][RX-C] 0.00-10.00 sec 1.05 GBytes 899 Mbits/sec receiver
iperf Done.
解決済! 解決策の投稿を見る。
So once more the kernel community turned out to be of much more avail than the NXP community. After I had posted my issue on the mailing lists it quickly turned out, that other people with different hardware were seeing the same problem.
Finally Joakim Zhang was kind enough to have a closer look and came up with the information that this is a known issue in relation to AVB support. There are three TX queues, but only the first one provides the full bandwidth. Queue 1 and 2 are limited to 50% of the nominal bandwidth. As the driver "randomly" chooses the queue, in about two thirds of the cases it selects one of the limited queues.
NXP has a patch in their downstream kernel, that solves this by preferring queue 0 for untagged, non-AVB traffic, but apparently nobody ever cared to upstream this so far.
Another quick workaround is to just disable the other queues by setting fsl,num-tx-queues = <1> in the devicetree, which obviously has the downside of not being able to handle the AVB traffic as intended.
So once more the kernel community turned out to be of much more avail than the NXP community. After I had posted my issue on the mailing lists it quickly turned out, that other people with different hardware were seeing the same problem.
Finally Joakim Zhang was kind enough to have a closer look and came up with the information that this is a known issue in relation to AVB support. There are three TX queues, but only the first one provides the full bandwidth. Queue 1 and 2 are limited to 50% of the nominal bandwidth. As the driver "randomly" chooses the queue, in about two thirds of the cases it selects one of the limited queues.
NXP has a patch in their downstream kernel, that solves this by preferring queue 0 for untagged, non-AVB traffic, but apparently nobody ever cared to upstream this so far.
Another quick workaround is to just disable the other queues by setting fsl,num-tx-queues = <1> in the devicetree, which obviously has the downside of not being able to handle the AVB traffic as intended.
Do you have the EVK and try the same test?
We have the EVK in the office. When I have some time I will try to test on that board.
I couldn't test on the NXP EVK so far, but we have some other hardware that uses the same Kontron i.MX8MM SoM, but with a KSZ8081 PHY connected via RMII (instead of RGMII) and I can see the same behavior there.