i.MX8MM ECSPI SS as GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM ECSPI SS as GPIO

510 Views
t_remmet
Contributor I

As on the i.MX8MM only SS0 is routed out externally, I wonder how many SS can be realized with GPIO per ecspi bus?

As there are 4 SS internally intended I suspect it should be save to use 4 chip selects also as GPIOs then. Is this correct?

Labels (1)
Tags (2)
0 Kudos
1 Reply

472 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

If you are willing to use the chip select with GPIOs. Theoretically, there is no limit. You just need to modify the ECSPI driver, since is configured in our BSP to use the SS0 for the ECSPI2.

Hope this information could help you.

Best regards,

Diego.  

0 Kudos