i.MX8MM Can't use HAB after SPL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM Can't use HAB after SPL

ソリューションへジャンプ
670件の閲覧回数
nunojpg
Contributor I

I have a locked board which loads the SPL fine.
SPL can then call imx_hab_authenticate_image which also succeeds if image properly signed, and fails if not.

But then I noticed that I could NOT authenticate a signed kernel from u-boot. I went back to try to call imx_hab_authenticate_image again just like SPL does (same addresses, so in fact to authenticate u-boot from u-boot), but it fails.
Some observations:

- when debugging hab.c, in see in SPL it takes the paths of current_el() == 3 and in u-boot of current_el() != 3.
- hab_status in u-boot always reads HAB Configuration: 0x00, HAB State: 0x00.
- Some basic SMC calls return this

=> smc C2000007 00
Res: 0 0 0 0
=> smc C2000007 01
Res: 240 1 0 0
=> smc C2000007 02
Res: 240 2 0 0
=> smc C2000007 03
Res: 51 3 0 0
=> smc C2000007 04
Res: 51 4 0 0
=> smc C2000007 06
Res: 51 6 0 0
=> smc C2000007 07
Res: 262921 7 0 0
=> smc C2000007 05

<hangs>

My problem is apparently that I can't talk to HAB when I drop from EL3.


SOC i.MX8M Mini
ATF v2.8
U-boot 2023.01

As I am using mainline versions and custom configs I don't expect to get a clear answer, but probably someone can point me what could be breaking this as I have no experience with ATF.

0 件の賞賛
返信
1 解決策
648件の閲覧回数
nunojpg
Contributor I
0 件の賞賛
返信
2 返答(返信)
637件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @nunojpg 

ATF mainline does not support HAB SIP, only ATF-NXP.

 

Best regards

Harvey

0 件の賞賛
返信
649件の閲覧回数
nunojpg
Contributor I
0 件の賞賛
返信