i.MX8MM外接LPDDR4是否支持,如何配置

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM外接LPDDR4是否支持,如何配置

2,329 Views
yongyang
Contributor I

我们使用I.MX8MM芯片外接了一片LPDDR4,但是无法烧写UBOOT启动,如下图

yongyang_0-1704256682070.jpeg

请各位大神给予帮助,救急!!!!

下面附有对应LPDDR4手册

Labels (1)
0 Kudos
Reply
9 Replies

2,116 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang

Please use the following link to download the new DDR Config Tool:

https://www.nxp.com/design/design-center/development-boards/i-mx-evaluation-and-development-boards/c...

B.R

 

0 Kudos
Reply

2,113 Views
yongyang
Contributor I
we have start up the ddr,thank you.
0 Kudos
Reply

2,218 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang 

Please re-run the ddr stress tool with the attached file.

B.R

0 Kudos
Reply

2,201 Views
yongyang
Contributor I

不行,板子跑不起来。

yongyang_0-1704447619856.jpeg

 

0 Kudos
Reply

2,293 Views
pengyong_zhang
NXP Employee
NXP Employee

hi, @yongyang 

Do you choose the right uart port? Please share the  Hardware schematic of the board.

 

B.R

0 Kudos
Reply

2,221 Views
yongyang
Contributor I
你好,原理图我已经发给您了
0 Kudos
Reply

2,240 Views
yongyang
Contributor I

hardware schematic of board have been uploded.

0 Kudos
Reply

2,306 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang 

I saw the ddr datasheet and it has two channels, but there is only one channel in your set.

please set Nummber of channels : 2, Number of Chip Selects used :1.

 

B.R

0 Kudos
Reply

2,297 Views
yongyang
Contributor I

yongyang_0-1704268732913.jpeg

按照您的指示配置了,还是不行呀。

 

0 Kudos
Reply