i.MX8MM外接LPDDR4是否支持,如何配置

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM外接LPDDR4是否支持,如何配置

1,148件の閲覧回数
yongyang
Contributor I

我们使用I.MX8MM芯片外接了一片LPDDR4,但是无法烧写UBOOT启动,如下图

yongyang_0-1704256682070.jpeg

请各位大神给予帮助,救急!!!!

下面附有对应LPDDR4手册

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

935件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang

Please use the following link to download the new DDR Config Tool:

https://www.nxp.com/design/design-center/development-boards/i-mx-evaluation-and-development-boards/c...

B.R

 

0 件の賞賛
返信

932件の閲覧回数
yongyang
Contributor I
we have start up the ddr,thank you.
0 件の賞賛
返信

1,037件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang 

Please re-run the ddr stress tool with the attached file.

B.R

0 件の賞賛
返信

1,020件の閲覧回数
yongyang
Contributor I

不行,板子跑不起来。

yongyang_0-1704447619856.jpeg

 

0 件の賞賛
返信

1,112件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

hi, @yongyang 

Do you choose the right uart port? Please share the  Hardware schematic of the board.

 

B.R

0 件の賞賛
返信

1,040件の閲覧回数
yongyang
Contributor I
你好,原理图我已经发给您了
0 件の賞賛
返信

1,059件の閲覧回数
yongyang
Contributor I

hardware schematic of board have been uploded.

0 件の賞賛
返信

1,125件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongyang 

I saw the ddr datasheet and it has two channels, but there is only one channel in your set.

please set Nummber of channels : 2, Number of Chip Selects used :1.

 

B.R

0 件の賞賛
返信

1,116件の閲覧回数
yongyang
Contributor I

yongyang_0-1704268732913.jpeg

按照您的指示配置了,还是不行呀。

 

0 件の賞賛
返信