i.MX8MINI board not Booting

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX8MINI board not Booting

Jump to solution
296 Views
PramodKumar
Contributor IV

We designed the i.MX8MINI based board the debug messages is given below

*************************************************************************************************************************

Debug Message Stat here:

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 (Oct 09 2019 - 05:57:03 +0000)
power_bd71837_init
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
"Synchronous Abort" handler, esr 0x96000000
elr: 00000000007e88ac lr : 00000000007e919c
x0 : 0000000042200250 x1 : 000000000091dbf0
x2 : 0000000000000000 x3 : 0000c000007f1900
x4 : 0000000000000000 x5 : 0000000000000000
x6 : 00000000401ffd95 x7 : 0000000000000003
x8 : 0000000000000064 x9 : 0000000000000002
x10: 000000000091db5c x11: 00000000401ff980
x12: 0000000000000064 x13: 0000000000000058
x14: 000000000091dc2c x15: 00000000401ff980
x16: 0000000000000000 x17: 00000000000000ff
x18: 000000000091de40 x19: 00000000000004ec
x20: 0000000042200250 x21: 00000000000004ec
x22: 00000000000004ec x23: 0000000000000318
x24: 0000000000000000 x25: 0000000040200000
x26: 00000000007f16f2 x27: 0000000000000011
x28: 0000000000000000 x29: 000000000091db70

Resetting CPU ...

resetting ...

Debug Message End here

*************************************************************************************************************************

Please helps us to get the correct root cause of issue of  "Synchronous Abort" handler" message.

Is this message is due to SD card channel not selected due to some hardware issue or DDR4 has some design issue.

Regards,

Pramod Kumar

0 Kudos
1 Solution
271 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!

View solution in original post

0 Kudos
2 Replies
272 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this discussion as solved, due to a migration of a new community platform.
If you have additional questions, please create a new post and reference to this closed thread.

NXP Community!

View solution in original post

0 Kudos
288 Views
david_dicarlo
NXP Employee
NXP Employee

This is not quite the right place to ask the question.  Please ask it here: https://community.nxp.com/community/imx 

0 Kudos