i.MX8M plus - MIPI CSI 2 supports packets with virtual channel ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M plus - MIPI CSI 2 supports packets with virtual channel ID

Jump to solution
2,957 Views
shai_b
Senior Contributor II

Dear Team,

My customer is planning to use two MT9M114 (from On-Semi) CMOS sensors and combine the two MIPI-CSI2 ports into one port (using Lattice FPGA device).

My question is, does i.MX8M Plus MIPI-csi2 interface knows to handle virtual channel ID and separate back the MIPI signal into two channels?
Waiting for your kind response, Thanks in advance

BR,
Shai

0 Kudos
Reply
1 Solution
2,952 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shai

 

unfortunately i.MX8M Plus MIPI-CSI hardware does not support virtual channels, sorry.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
4 Replies
2,482 Views
M-tech
Contributor I

Dear Team,
Which of your processors does accept virtual channel for mipi-csi2 interface?
Thanks

0 Kudos
Reply
2,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shai

 

unfortunately i.MX8M Plus MIPI-CSI hardware does not support virtual channels, sorry.

 

Best regards
igor

0 Kudos
Reply
1,246 Views
AlexSobko
Contributor I

i.MX8M IMX8MPLUS

Hi Igor,

Is this still true now in 2024?

Are there any future plans for adding the CSI-2 virtual channels support in i.MX8M plus or any other i.MX family processors?

Thanks,

Alex

Tags (1)
0 Kudos
Reply
2,944 Views
shai_b
Senior Contributor II

@igorpadykov ,

Thank you for your feedback.

KR,

Shai

0 Kudos
Reply