i.MX8M mini - QSPI/FlexSPI as Master <=> FPGA as Slave

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX8M mini - QSPI/FlexSPI as Master <=> FPGA as Slave

1,476 Views
sherlock_hsia
Contributor I

i.MX8M mini - QSPI/FlexSPI as Master <===>  FPGA - QSPI/FlexSPI as Slave.

Dear Sir,

Our project want to use i.MX8M mini - QSPI/FlexSPI as Master mode,

and FPGA - QSPI/FlexSPI as Slave.

Could you help us: the information on S.W. reference code/reference manual.

Thanks,

0 Kudos
5 Replies

602 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Sherlock

example can be found in linux/arch/arm64/boot/dts/freescale/fsl-imx8mm-ddr4-val.dts

fsl-imx8mm-ddr4-val.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

fsl-flexspi.c\spi-nor\mtd\drivers - linux-imx - i.MX Linux kernel 

qspi driver is described in sect.3.5 Quad Serial Peripheral Interface (QuadSPI)

Linux Manual included in Linux L4.14.98_2.0.0 Documentation


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

602 Views
tberryhill
Contributor I

Igor,

The flexspi driver uses the spi_nor structure which is a memory specific data structure. How can the fsl-flexspi.c driver be used to implement the simple hardware configuration mentioned by Sherlock on an i.MX8M Mini?

0 Kudos

602 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Tyler

if it is fpga it can imitate memory.

Best regards
igor

0 Kudos

602 Views
ywm
Contributor I

Igor,
Do you has this QSPI interface example or reference design by FPGA for this discussion? or can share more about the imitate memory method?

Thanks

HugoY

0 Kudos

602 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Hugo


>Do you has this QSPI interface example or reference design by FPGA for this discussion?

>or can share more about the imitate memory method?

sorry such example is not available.

 

Best regards
igor
0 Kudos