i.MX8M mini: CCM_CLK02

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M mini: CCM_CLK02

ソリューションへジャンプ
1,779件の閲覧回数
saidjazouly
Contributor III

Hello NXP,

We have designed a board based on the i.MX8M mini reference design.

Our customer would like to output a clock of 24MHz on CCM_CLK02 pad AB9 of the chip

 

saidjazouly_0-1605134081242.png

  1. What is the configuration needed to be done in the dts or any other relevant code to output the 24MHz?
  2. Is it possible to output this clock @24MHz in Linux only or in both u-boot and Linux?

Best regards!

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,755件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

No matter which version of bsp, you can modify the clock driver manually. However, do not copy these codes directly. Because each version will be different.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,756件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

No matter which version of bsp, you can modify the clock driver manually. However, do not copy these codes directly. Because each version will be different.

0 件の賞賛
返信
1,774件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  Try below, please!

--------------------------------

diff --git a/drivers/clk/imx/clk-imx8mm.c b/drivers/clk/imx/clk-imx8mm.c
index 5709bfce578c..2ef53f153728 100644
--- a/drivers/clk/imx/clk-imx8mm.c
+++ b/drivers/clk/imx/clk-imx8mm.c
@@ -404,6 +404,9 @@ static struct clk ** const uart_clks[] __initconst = {
static const char *imx8mm_clko1_sels[] = {"osc_24m", "sys_pll1_800m", "osc_27m", "sys_pll1_200m", "audio_pll2_clk",
"vpu_pll", "sys_pll1_80m", };

+static const char *imx8mm_clko2_sels[] = {"osc_24m", "sys_pll2_200m", "sys_pll1_400m", "sys_pll2_166m", "sys_pll3_out",
+ "audio_pll1_clk", "vpu_pll_out", "osc_32k", };
+
static int __init imx_clk_init_on(struct device_node *np,
struct clk * const clks[])
{
@@ -665,6 +668,7 @@ static void __init imx8mm_clocks_init(struct device_node *ccm_node)
clks[IMX8MM_CLK_WDOG_SRC] = imx_clk_mux2("wdog_src", base + 0xb900, 24, 3, imx8mm_wdog_sels, ARRAY_SIZE(imx8mm_wdog_sels));
clks[IMX8MM_CLK_WRCLK_SRC] = imx_clk_mux2("wrclk_src", base + 0xb980, 24, 3, imx8mm_wrclk_sels, ARRAY_SIZE(imx8mm_wrclk_sels));
clks[IMX8MM_CLK_CLKO1_SRC] = imx_clk_mux2("clko1_src", base + 0xba00, 24, 3, imx8mm_clko1_sels, ARRAY_SIZE(imx8mm_clko1_sels));
+ clks[IMX8MM_CLK_CLKO2_SRC] = imx_clk_mux2("clko2_src", base + 0xba80, 24, 3, imx8mm_clko2_sels, ARRAY_SIZE(imx8mm_clko2_sels));
clks[IMX8MM_CLK_DSI_CORE_SRC] = imx_clk_mux2("dsi_core_src", base + 0xbb00, 24, 3, imx8mm_dsi_core_sels, ARRAY_SIZE(imx8mm_dsi_core_sels));
clks[IMX8MM_CLK_DSI_PHY_REF_SRC] = imx_clk_mux2("dsi_phy_ref_src", base + 0xbb80, 24, 3, imx8mm_dsi_phy_sels, ARRAY_SIZE(imx8mm_dsi_phy_sels));
clks[IMX8MM_CLK_DSI_DBI_SRC] = imx_clk_mux2("dsi_dbi_src", base + 0xbc00, 24, 3, imx8mm_dsi_dbi_sels, ARRAY_SIZE(imx8mm_dsi_dbi_sels));
diff --git a/include/dt-bindings/clock/imx8mm-clock.h b/include/dt-bindings/clock/imx8mm-clock.h
index 083dd6d0116d..0745122611ca 100644
--- a/include/dt-bindings/clock/imx8mm-clock.h
+++ b/include/dt-bindings/clock/imx8mm-clock.h
@@ -469,5 +469,7 @@
#define IMX8MM_CLK_NAND_USDHC_BUS_RAWNAND_CLK 455
#define IMX8MM_CLK_SIM_HSIO 456

-#define IMX8MM_CLK_END 457
+#define IMX8MM_CLK_CLKO2_SRC 457
+
+#define IMX8MM_CLK_END 458
#endif
--

-----------------------------------------------

Hope it is helpful to you.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信
1,764件の閲覧回数
saidjazouly
Contributor III

Thank you Sun for your reply!

 

  1. Can you please tell me what kernel version is the diff generated from?
  2. Do you have a more recent patch based on kernel 5.4.24?

Best regards.

0 件の賞賛
返信