i.MX8M mini CAAM and SNVS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M mini CAAM and SNVS

1,201 Views
antonio_santagi
Contributor IV

Hello

can the CAMM Cryptographic Acceleration and Assurance Module and SNVS Secure Non-Volatile Storage hw modules in iMx8MMini considered equivalent in features and performance to a TPM ?

Can I achieve with them the same or better security level than with an external TPM module ?

thank you

0 Kudos
3 Replies

1,101 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly some comments.

Regards,

Yuri.

0 Kudos

882 Views
AlfTeleco
Contributor III

Hello, 

We are designing a custom iMX8MP platform and are very interesting in the need of including a separate TPM. Do CAAM and SNVS enable the same features as a TPM does?

 

Thanks in advance

0 Kudos

1,101 Views
djoh
Contributor I

Hello,

I'm interested in this topic as well. Would you be so kind to pass the information to me, too?

Best regards

0 Kudos