Trying to find more details around the frame classification (see from manual below)
Can I for instance filter so that time-sensitive ends up in its own buffer and IRQ,
thus allowing core-isolation so TSN/AVB traffic could be tied to the M7 while L3 traffic is passed to the A53?

Would also like some guidance to either code or more in-depth documentation for the two different PHY's in the imx8plus, there are obviously two variants of the IP's used for phy0 vs phy1. I'd like to understand
- what features are supported on each
- more details how fifo's/queues and irq's are segmented
thanks