Hello, i.MX community!
I'm examining i.MX8M Plus SoC for our project and try to run basic GStreamer tests.
I've demo video file with the following parameters:
Stream #0:0(eng): Video: hevc (Main) (hvc1 / 0x31637668), yuv420p(tv), 1920x1080, 36173 kb/s, 29.97 fps, 29.97 tbr, 30k tbn, 29 tbc (default)
Which successfully processed by this command on my PC:
$ gst-launch-1.0 filesrc location=demo_with_text.mp4 ! decodebin ! textoverlay font-desc="Sans 20" text="Hello world!" shaded-background=false ! x264enc ! mp4mux name=mp4mux ! filesink location=demo_with_text.mp4
But on i.MX8M Plus I have very weird issues:
$ gst-launch-1.0 filesrc location=demo.mp4 ! decodebin ! textoverlay font-desc="Sans 20" text="Hello world!" shaded-background=false ! vpuenc_h264 ! mp4mux name=mp4mux ! filesink location=demo_with_text.mp4
Setting pipeline to PAUSED ...
====== VPUENC: 4.7.0 build on May 20 2022 06:51:21. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jun 2 2022 08:51:59)
vpulib: 1.1.1
firmware: 1.1.1.43690
Pipeline is PREROLLING ...
====== AIUR: 4.7.0 build on May 20 2022 06:51:21. ======
Core: MPEG4PARSER_06.20.06 build on May 7 2022 07:52:31
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:11:24.684000000
Language: und
Mime:
video/x-h265, parsed=(boolean)true, alignment=(string)au, stream-format=(string)hev1, width=(int)1920, height=(int)1080, framerate=(fraction)30000/1001, codec_data=(buffer)01014000000080000000000078f000fcfdf8f800000f03200001002240010c01ffff014000000300800000030000030078ac0c00000fa00001c52200fa28210001002a420101014000000300800000030000030078a003c08010e7fa2eec9577a25d581000003e800007148c4022000100074401c1adf01364
------------------------
====== VPUDEC: 4.7.0 build on May 20 2022 06:51:21. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jun 2 2022 08:51:59)
vpulib: 1.1.1
firmware: 1.1.1.65535
VCEncCheckCfg: Invalid frameRateNum
VCEncInit: ERROR Invalid configuration
ERROR: from element /GstPipeline:pipeline0/GstDecodeBin:decodebin0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.
Additional debug info:
../git/plugins/aiurdemux/aiurdemux.c(1139): aiurdemux_pull_task (): /GstPipeline:pipeline0/GstDecodeBin:decodebin0/GstAiurDemux:aiurdemux0:
streaming stopped, reason error, state 3
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
I've converted my video to these parameters:
Stream #0:0(eng): Video: h264 (High) (avc1 / 0x31637661), yuv420p(tv, bt709), 1920x1088 [SAR 136:135 DAR 16:9], 1121 kb/s, 29.97 fps, 29.97 tbr, 2997 tbn, 59.94 tbc (default)
And GStreamer results are weird, the output file was 595 bytes!
$ gst-launch-1.0 filesrc location=demo.mp4 ! decodebin ! videoscale ! video/x-raw, format=NV12, width=640, height=480 ! textoverlay font-desc="Sans 20" text="Hello world!" shaded-background=false ! vpuenc_h264 ! mp4mux name=mp4mux ! filesink location=demo_with_text.mp4
Setting pipeline to PAUSED ...
====== VPUENC: 4.7.0 build on May 20 2022 06:51:21. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jun 2 2022 08:51:59)
vpulib: 1.1.1
firmware: 1.1.1.43690
Pipeline is PREROLLING ...
====== AIUR: 4.7.0 build on May 20 2022 06:51:21. ======
Core: MPEG4PARSER_06.20.06 build on May 7 2022 07:52:31
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:11:24.684017000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)1088, framerate=(fraction)333/11, codec_data=(buffer)01640828ffe1002067640828acd940780226ffc0220021da808080a000007d20001d4c11e30632c001000568ebecb22c
------------------------
====== VPUDEC: 4.7.0 build on May 20 2022 06:51:21. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jun 2 2022 08:51:59)
vpulib: 1.1.1
firmware: 1.1.1.65535
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
Redistribute latency...
New clock: GstSystemClock
Got EOS from element "pipeline0".
Execution ended after 0:00:00.001104000
Setting pipeline to NULL ...
Freeing pipeline ...