i.MX8M-Plus MPU component changes for custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M-Plus MPU component changes for custom board

271件の閲覧回数
Wobaffet
Senior Contributor I

MicrosoftTeams-image (3).png

MicrosoftTeams-image (2).png

Hello, is it possible to make the changes at the images in the square windows on our custom board for production and purchasing purposes?

  • 1uF 6.3V instead of 0.22uF 10V
  • 10 uF 10V instead of 4.7uF 6.3V
  • 22uF 10V instead of 10uF 16V
  • 10uF 10V instead of 1uF 10V and 4.7uF 10V
  • 10uF 10V instead of 1uF 10V
  • 22uF 10V instead of 10uF 16V
  • 10 uF 10V instead of 4.7uF 10V and 6.3V

0 件の賞賛
返信
0 返答(返信)