[i.MX8M Plus] IMX8MP EVK/switch uart4 to A53 and change debug console from uart2 to uart1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX8M Plus] IMX8MP EVK/switch uart4 to A53 and change debug console from uart2 to uart1

1,346 Views
sophiehu
Contributor III

Hi NXP,

I want to change switch uart4 to A53 and change debug console from uart2 to uart1.
I have referenced these two pages:
https://community.nxp.com/t5/Blogs/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40

https://community.nxp.com/t5/i-MX-Processors/IMX8MP-EVK-Change-u-boot-debug-console-UART2-gt-UART1/m...

I follow the patch in link above to modify in, except
+++ rel_imx_5.4.70_2.3.0_uart4/imx-atf/plat/imx/imx8m/imx8mm/include/platform_def.h 2021-03-10 16:57:07.299870347 +0800

@@ -51,7 +51,7 @@
 
 #define HAB_RVT_BASE           U(0x00000900) /* HAB_RVT for i.MX8MM */
 
-#define IMX_BOOT_UART_BASE     U(0x30890000)
+#define IMX_BOOT_UART_BASE     U(0x30a60000)
 
I found IMX_BOOT_UART_BASE defined in platform.mk, so I modify in platform.mk.
/plat/imx/imx8m/imx8mp/platform.mk b/plat/imx/imx8m/imx8mp/platform.mk



Environments:
SW: SDK 5.10.72_2.2.0
HW: imx8mp evk

Build SDK 5.10.72_2.2.0 with core image
$ bitbake core-image-base
Build SDK and install toolcahin
$ bitbake meta-toolchain
Copy imx-atf, u-boot-imx, imx-boot, linux-imx from SDK to outside for building standalone.

For u-boot:
I modify imx-atf and u-boot-imx as attached patch files and build standalone with command:
$ source /opt/fsl-imx-xwayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux
1. build imx-atf
    $ unset LDFLAGS
    $ make PLAT=imx8mp bl31
2. build u-boot
    $ export ARCH=arm64
    $ make clean
    $ make imx8mp_evk_defconfig
    $ unset LDFLAGS
    $ make
3. copy files to imx-boot
    $ cp imx-atf/build/imx8mp/release/bl31.bin imx-boot/iMX8M
    $ cp u-boot-imx/u-boot-nodtb.bin imx-boot/iMX8M
    $ cp u-boot-imx/arch/arm/dts/imx8mp-evk.dtb imx-boot/iMX8M
    $ cp u-boot-imx/spl/u-boot-spl.bin imx-boot/iMX8M
4. build imx-boot to generate flash.bin
    $ export ARCH=arm64
    $ make SOC=iMX8MP flash_spl_uboot
5. write flash.bin in sdcard
    To write release image in sdcard with uuu first, then write flash.bin with dd command.
    $ sudo dd if=imx-boot/iMX8M/flash.bin of=/dev/sdb bs=1k seek=32 conv=sync

For kernel:
I modify linux-imx as attached patch file and build standalone with command:
$ source /opt/fsl-imx-xwayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux
1. build kernel
    $ export ARCH=arm64
    $ make clean
    $ make imx_v8_defconfig
    $ make
2. replace Image and dtb in boot partition of sdcard
    $ sudo cp linux-imx/arch/arm64/boot/Image /media/<user>/boot
    $ sudo cp linux-imx/arch/arm64/boot/dts/freescale/imx8mp-evk.dtb /media/<user>/boot
    $ sudo umount /media/<user>/boot
    $ sudo umount /media/<user>/root

Finally boot from sdcard:
Connect debug port with micro-usb cable to PC.
Launch four terminals for those four COM ports.
It should boot successfully becase I can see the login terminal in uart1 after power on for a while.
However, I cannot see any debug messages in all the four COM ports.

sophiehu_0-1650615343001.png

What cound I miss?
Please help me to make it work correctly.

Best Regards,



0 Kudos
Reply
2 Replies

195 Views
senderovichadi
Contributor I

hi,

senderovichadi_0-1721201733154.png

 

sophiehu how did you solve the issue? 
 
In what file does IMX_BOOT_UART_BASE needs to be changed?
I am working with iMX8m Plus with distro version 6.1-mickledore
 
thanks
A
0 Kudos
Reply

1,319 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The only change that you have done differently may be causing this, could you share which version of imx-atf are you using?

In 5.4.70_2.3.0 it is indeed defined at plat/imx/imx8m/imx8mp/include/platform_def.h
https://source.codeaurora.org/external/imx/imx-atf/tree/plat/imx/imx8m/imx8mp/include/platform_def.h...

Best regards,
Aldo.

0 Kudos
Reply