i.MX8M Plus H.265 encoder - max possible resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Plus H.265 encoder - max possible resolution

5,888 Views
artsiomstaliaro
Contributor IV

Hello,

I'm facing a fact that vpuenc_hevc (plugin in GStreamer) has width: [ 64, 1920 ] and height: [ 64, 1088 ] parameter limitation to 1920x1088. 

But vpudec has width: [ 1, 2147483647 ] and height: [ 1, 2147483647 ] parameters - no limitation.

Is it i.MX8MPlus hardware limitation to 1920x1088 of the encoder? (can't find information in the documents)
Can I run 2160p encoding somehow?

CPU: i.MX8M Plus Quad

Labels (3)
0 Kudos
Reply
10 Replies

4,610 Views
briandavidson1
Contributor II

So it supports 60fps at 2MP. Can it support 30fps at 4MP and 15 fps 8MP like that?

0 Kudos
Reply

4,604 Views
artsiomstaliaro
Contributor IV
No, only 1920x1088 max. The resolution is fixed as far as i can see.
0 Kudos
Reply

4,620 Views
briandavidson1
Contributor II

Okay so it supports 2MP at 60fps, so can it support 4MP at 30fps?

0 Kudos
Reply

4,611 Views
artsiomstaliaro
Contributor IV
No, there HW limitation in resolution to 1920 x 1088 max.
0 Kudos
Reply

5,860 Views
artsiomstaliaro
Contributor IV

We modified 

imx-gst1.0-plugin, but still receiving during GStreamer (in case of higher resolution than 1920x1088) :

VCEncCheckCfg: Invalid width, not supported by HW coding core
VCEncCheckCfg: Invalid coding configuration for HW
VCEncInit: ERROR Invalid configuration

0 Kudos
Reply

5,849 Views
joanxie
NXP TechSupport
NXP TechSupport

as I mentioned before, this is should be software control limitation, but we don't have any patch for 4k support, and I can say, the 4k performance is very bad, so I don't suggest you waste time on this

0 Kudos
Reply

5,839 Views
artsiomstaliaro
Contributor IV

Our customer needs 4K encoded video even with 5-7fps.

0 Kudos
Reply

5,818 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry, we don't support this resolution, if you need customized this, maybe you can consult professional service to get more detailed information, but I'm not sure if we can support this though encoder IP can support this

"https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and..."

0 Kudos
Reply

5,882 Views
artsiomstaliaro
Contributor IV

Found this discussion https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Hantro-4K-Encoder/m-p/1282890

 

Seems need to modify the plugin to remove this limit.

0 Kudos
Reply

5,872 Views
joanxie
NXP TechSupport
NXP TechSupport

this is just based on theory, but now, I can say, imx8mp supports up to 1080p@60

0 Kudos
Reply