i.MX8M Plus H.265 encoder - max possible resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Plus H.265 encoder - max possible resolution

5,876件の閲覧回数
artsiomstaliaro
Contributor IV

Hello,

I'm facing a fact that vpuenc_hevc (plugin in GStreamer) has width: [ 64, 1920 ] and height: [ 64, 1088 ] parameter limitation to 1920x1088. 

But vpudec has width: [ 1, 2147483647 ] and height: [ 1, 2147483647 ] parameters - no limitation.

Is it i.MX8MPlus hardware limitation to 1920x1088 of the encoder? (can't find information in the documents)
Can I run 2160p encoding somehow?

CPU: i.MX8M Plus Quad

ラベル(3)
0 件の賞賛
返信
10 返答(返信)

4,598件の閲覧回数
briandavidson1
Contributor II

So it supports 60fps at 2MP. Can it support 30fps at 4MP and 15 fps 8MP like that?

0 件の賞賛
返信

4,592件の閲覧回数
artsiomstaliaro
Contributor IV
No, only 1920x1088 max. The resolution is fixed as far as i can see.
0 件の賞賛
返信

4,608件の閲覧回数
briandavidson1
Contributor II

Okay so it supports 2MP at 60fps, so can it support 4MP at 30fps?

0 件の賞賛
返信

4,599件の閲覧回数
artsiomstaliaro
Contributor IV
No, there HW limitation in resolution to 1920 x 1088 max.
0 件の賞賛
返信

5,848件の閲覧回数
artsiomstaliaro
Contributor IV

We modified 

imx-gst1.0-plugin, but still receiving during GStreamer (in case of higher resolution than 1920x1088) :

VCEncCheckCfg: Invalid width, not supported by HW coding core
VCEncCheckCfg: Invalid coding configuration for HW
VCEncInit: ERROR Invalid configuration

0 件の賞賛
返信

5,837件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

as I mentioned before, this is should be software control limitation, but we don't have any patch for 4k support, and I can say, the 4k performance is very bad, so I don't suggest you waste time on this

0 件の賞賛
返信

5,827件の閲覧回数
artsiomstaliaro
Contributor IV

Our customer needs 4K encoded video even with 5-7fps.

0 件の賞賛
返信

5,806件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

sorry, we don't support this resolution, if you need customized this, maybe you can consult professional service to get more detailed information, but I'm not sure if we can support this though encoder IP can support this

"https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and..."

0 件の賞賛
返信

5,870件の閲覧回数
artsiomstaliaro
Contributor IV

Found this discussion https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-Hantro-4K-Encoder/m-p/1282890

 

Seems need to modify the plugin to remove this limit.

0 件の賞賛
返信

5,860件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this is just based on theory, but now, I can say, imx8mp supports up to 1080p@60

0 件の賞賛
返信