i.MX8M Nano Secure Boot (HABv4) UUU Tool Flash Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8M Nano Secure Boot (HABv4) UUU Tool Flash Error

778 次查看
Nethaji1510
Contributor II

Hello,

We are working with two different hardware boards with the i.Mx8M Nano processor. We have successfully enabled secure boot on both boards using the following command:
              $ fuse prog 1 3 0x02000000


Both boards successfully booted up with signed images.

Issue: While we were able to flash the new signed firmware onto Board 1 via USB using the UUU command, we were not able to do so on Board 2

Query: We used the same UUU tool to flash both boards. Could there be any hardware pin configurations (e.g., GPIO HIGH/LOW) that need to be adjusted to enable USB flashing via the UUU tool on Board 2?

0 项奖励
回复
1 回复

725 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Seems the boot mode is not in USB download mode. Please check the boot mode of the board 2.

0 项奖励
回复